2019-07-12 5:00 AM
Hai, I am using stm32f429igt controller I am trying to use IAP and found one example with stm32f4 cube package. While trying the example the code is not getting uploaded when I tried to upload it still waiting for the file can anyone help me how to solve this.
2019-07-12 6:00 AM
You need to use Y-Modem to send a binary file, not send a string of hex codes.
2019-07-12 9:20 PM
Ya I am using Y-Modem to receive the binary file which i generated from the keil IDE. When it waiting for the file I am sending the file using Hercules terminal after it is send it still waiting for the file if i send it twice it goes into hard fault handler. Is that anything else i have to add to the binary file generated to end the transmission...?? (i.e) the file is successfully received.
void SerialDownload(void)
{
uint8_t Number[10] = " ";
int32_t Size = 0;
SerialPutString("Waiting for the file to be sent ... (press 'a' to abort)\n\r");
Size = Ymodem_Receive(&tab_1024[0]);
if (Size > 0)
{
SerialPutString("\n\n\r Programming Completed Successfully!\n\r--------------------------------\r\n Name: ");
SerialPutString(FileName);
Int2Str(Number, Size);
SerialPutString("\n\r Size: ");
SerialPutString(Number);
SerialPutString(" Bytes\r\n");
SerialPutString("-------------------\n");
}
else if (Size == -1)
{
SerialPutString("\n\n\rThe image size is higher than the allowed space memory!\n\r");
}
else if (Size == -2)
{
SerialPutString("\n\n\rVerification failed!\n\r");
}
else if (Size == -3)
{
SerialPutString("\r\n\nAborted by user.\n\r");
}
else
{
SerialPutString("\n\rFailed to receive the file!\n\r");
}
}
2019-07-12 10:46 PM
Hi i just now figured out what you said that i have send the binary file using Y-Modem protocol. Now i have used hyper terminal to send the file using Y-Modem protocol but in his also i am getting some error when sending the file below i have attached the screen short of my error.