2017-08-24 2:40 PM
Hello. I am trying to perform I2C communication between the stm32f429 disco board and an arduino mega adk. When I used my debugger I found that my code gets stuck in the while loop inside the send_data function infinitely. Although my led on pg13 is lighting up, I feel that the arduino isn't actually sending an acknowledge. Any help would be greatly appreciated.
void led_init1()
{ RCC ->AHB1ENR |= RCC_AHB1ENR_GPIOGEN; GPIOG ->MODER |= GPIO_MODER_MODER13_0; GPIOG ->OTYPER &= ~(GPIO_OTYPER_OT_13); GPIOG ->OSPEEDR |= GPIO_OSPEEDER_OSPEEDR13_0; GPIOG ->PUPDR &= ~(GPIO_PUPDR_PUPDR13); }void scl_pin()
{ RCC ->AHB1ENR |= RCC_AHB1ENR_GPIOBEN; GPIOB ->MODER |= GPIO_MODER_MODER6_1; GPIOB ->AFR[0] = GPIO_AF4_I2C1<<24;}void sda_pin(){ RCC ->AHB1ENR |= RCC_AHB1ENR_GPIOBEN; GPIOB ->MODER |= GPIO_MODER_MODER7_1; GPIOB ->OTYPER &= ~(GPIO_OTYPER_OT_7); GPIOB ->OSPEEDR |= GPIO_OSPEEDER_OSPEEDR7_1; GPIOB ->PUPDR |= GPIO_PUPDR_PUPDR7_0; GPIOB ->AFR[0] = GPIO_AF4_I2C1<<28;}void i2c_setup(){ RCC->APB1ENR |= RCC_APB1ENR_I2C1EN; I2C1 ->CR2 |= I2C_CR2_FREQ_3; I2C1 ->CCR |= 0x28; I2C1 ->TRISE = 0x09;I2C1 ->CR1 |= I2C_CR1_PE;
I2C1 ->CR1 |= I2C_CR1_ACK; I2C1 ->CR1 |= I2C_CR1_START; I2C1 ->DR = 0x08;}void send_data(uint8_t data)
{ while(!(I2C1->SR1 & I2C_SR1_TXE)){} I2C1 ->DR = data;}
int main(void){ led_init1(); scl_pin(); sda_pin(); i2c_setup(); if(I2C1->CR1 & I2C_CR1_ACK) GPIOG ->BSRRL |= GPIO_BSRR_BS_13; while(1) { send_data(5); }}#i2c #stm322017-08-24 5:56 PM
The number of people wanting to wade through this kind of code is fairly small.
Put a scope on the pins, and inspect the waveforms.
Make sure you have the pins configured in OD (Open Drain) mode, with internal or external pull-ups.
Make sure the boards share a common ground.