cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f429 discovery dfu problem

er3481
Senior
Posted on April 21, 2016 at 12:19

Hi,

I want to use bootloader from usb with stm32f429 discovery board. I have pull down the BOOT0 pin and pull up the BOOT1(PB2) pin. I have connected the boards to copmuter from usb connectors (from mini and micro usb) but i can not see the board as ''stm device in dfu mode'' in device manager. what can the solution be ?
2 REPLIES 2
Posted on April 21, 2016 at 13:20

I don't believe the ROM supports DFU vis the USB_HS interface.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
er3481
Senior
Posted on April 21, 2016 at 13:30

why not? do you think that it is not possible with stm32f429 mcu or with discovery board?