cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F429 and STM32F469 FMC limitations

bluephoton928
Associate II
Posted on January 22, 2016 at 18:19

Hi Does any one know the minimum lead count device I need to choose on STM32F429 to ensure it supports SDR SDRAM memory? In the datasheet it only mentions 100L can only support PSRAM and some other Flash based.

I would like to know what types of memories are supported by FMC on each of these pin counts offered on STM32F429 & STM32F469

100L

143L

144L

169L

176L

208L

216L

#stm32f429-fmc
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Nesrine M_O
Lead II
Posted on January 25, 2016 at 14:06

Hi henry.blue,

In STM32F429/469 datasheets, in the Pinouts and pin description section you find a summary table about FMC pin definition on different supported memories. 

Based on this table and using STM32CUBEMX you can easily identify supported memories on FMC interface per package  

-Syrine-

bluephoton928
Associate II
Posted on January 26, 2016 at 18:29

Hi Syrine,

The FMC table was not very helpful as I dont know much about the STM32CUBEMX. Could you tell me the minimum pincount device to pick from STM32F429 if I were to interface with an external SDR SDRAM? The same question applies to STM32F469.

Thanks for the help,

HB

Radosław
Senior III
Posted on January 26, 2016 at 18:34

Please use CubeMX. this will take you a few minutes.