STM32F412RGT6 adc problem
- November 29, 2023
- 1 reply
- 1384 views
Hello all,
i am facing a problem while wokring with adc on stm32f412rgt6. i am facing problem of adc accuracy i am using 5 analog channel (ADC1_AN1, ADC1_AN10, ADC1_AN11, ADC_AN12, ADC_AN13) in discontinous mode.
when i am connecting analog input pin to ground, digital outout varies from 10-25 and linearity with input voltage change is also not good.
while trying multiple this and that to solve this problem i found when i use sysTick as timebase source then average digital output varies from 1-4 and when any other timer as in my case it is TIM4 then average digital output varies from 10-25.
here i am taking average of 200 adc samples per second.
i have to use systick for FREERTOS tick so i have to any other timer as timebase source.
i have to C files for your reference.
Thank you.