cancel
Showing results for 
Search instead for 
Did you mean: 

[STM32F412] Changing system clock issue

MB.2
Associate III

I am trying to change the system clock on my STM32F412 discovery board to 100 MHz using the HSI, however it just seems to crash. I am using direct writes to registers, but I looked at pregenerated CubeMX code and my registers look the same for the clock settings.

It crashes when I try to run the application on the board. Ignore the for loops in my code, they were just there for debugging stuff.

I do the following (HSI is selected by default):

Enable the Power control in the APB1

Set to scale 3 since I want it at 100 MHz

Turn the PLL off

Set PLLM to 8, PLLN to 0x64, PLLQ to 3, PLLR to 2, PLLP to 0

Set PPRE to 4 and SW to 2

Turn the PLL on and the adjustment

Wait for PLL to be ready

Wait for Power to be ready

int i;
 
	RCC_APB1EN_R |= APB1EN_PWREN;
 
	PWR_C_R = PWR_C_VOS_SCALE3;
	for(i = 0; i < 500; i++);
 
 
	RCC_C_R &= ~C_PLLON;
	for(i = 0; i < 500; i++);
 
	RCC_PLLCFG_R = PLLCFG_PLLM_8 | PLLCFG_PLLN_64 | PLLCFG_PLLQ_3 | PLLCFG_PLLR_2 | PLLCFG_PLLP_0;
	for(i = 0; i < 500; i++);
 
	RCC_CFG_R = CFG_PPRE1_4 | CFG_SW_2;
	for(i = 0; i < 500; i++);
 
 
	RCC_C_R = C_PLLON | C_HSITRIM_10;
 
 
 
	while(!(RCC_C_R & C_PLLRDY));
 
	while(!(PWR_CS_R & PWR_CSR_VOSRDY));

I confirm this doesn't work, I get a crash. I checked all my registers and they seem to be the same as the CubeMX generated project but I need to use registers writes for this because it is for a project and we are forbidden from an external API.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Uwe Bonnes
Chief

You need to set the needed flash wait cycles before switching up speed!

Wow! I am silly! I completely overlooked that. That fixed it. Thank you so much!