cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F411 Output pin connection while no VCC is applied

Nir Alon
Associate II
Posted on April 01, 2018 at 13:22

Hello all,

In my application, I'm controlling a

secondary 

device using enable pin which has an internal pull-up resistor.

The output pin is set to be ''0'' or open drain type output, and the STM32F411 VCC1 can be powered down while the

secondary 

device's VCC2 is still active.0690X00000604X3QAI.jpg

Can I connect the output pin directly to the secondary device enable pin or should I place a Tri-state buffer between them?

Thanks!

Nir

This discussion is locked. Please start a new topic to ask your question.
17 REPLIES 17
T J
Lead
Posted on April 02, 2018 at 10:03

easy enough with a transistor or Fet,

do you want it to operate only when you are powered up ?

then you need to signal high to indicate ON

use a BC817 with a 1k from the processor to the base.

this way the trigger can only operate when the processor is up.

Posted on April 02, 2018 at 10:29

I will rephrase the question - can the stm32f411 output handle (In terms of damage) the 3.3V VCC2 voltage (coming through the pull-up resistor) while VCC1 is 0V?

Posted on April 02, 2018 at 14:20

It use to be, that a pin will draw current if it gets to 1.2V (ish), and appear as a low voltage drive pin.

Please correct me guys, I know you will...

but I think you will power the processor 3V rail from the protection diodes within the pin IO structure.

thereby sinking 20mA or more which may take out the pin after a short period.

other than that, I think you will be ok..

Posted on April 02, 2018 at 15:50

Hi

I just came across this figures (page 60 - DocID026289 Rev 7):

0690X0000060AMpQAM.png 

If I understand correctly, than if VDD=0 I can apply 4.0V at any pin safely without any damage to the pin.

(In my case it would be 3.3V through a 100K pull-up resistor)

Am I right?

Nir

Posted on April 02, 2018 at 16:01

with a 100k. that's 10uA per volt.

that's 20uA flowing into the pin, charging it to where the protection diodes will start to conduct

clamping it down to roughly 1.2V

should be ok, I guess.

did you try it ?

what will your drive do at 1.2V ?

LMI2
Lead
Posted on April 02, 2018 at 19:46

CPUs have a common earth I suppose? Some chips may boot up badly if there is already current flowing into one pin when VCC is rising.

Posted on April 03, 2018 at 02:41

But look at Note 1 beneath the table ...

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
Posted on April 04, 2018 at 07:01

1. CPUs have a common ground

2. Yes, I build it and and while the VCC1 MCU is on, the output changes between 0 - 3.3V as expected, and when the VCC1 MCU is off, I measured 3.3V coming from the secondary MCU. Powering up the VCC1 MCU again was just fine.

3. Andrew, did I missed something in note 1? isn't it obvious that VDD, VSS should work in the permitted range?

Thanks again guys,

Nir

Nir Alon
Associate II
Posted on April 04, 2018 at 11:17

So...the only pin that can accept voltage while VCC=0 is BOOT0?