2016-03-07 12:53 PM
Hello. I am trying to get PA7 gpio port to work but it is not working not as input neither as output (i havent checked alternate functions). When i read or write from it the result is 0. There is a possibility that i may have shorted it to GND or connected to a 9V battery, while it was in high state as output. It is dead ins't it? I checked many other pins and they seem to function properly.
2016-03-07 01:53 PM
As the only person with your part, and knowing what else it is connected too, you are probably best positioned to understand if it is destroyed or not.
I'm not sure what you're looking for here. If you have destroyed the IO pad, not much can be done to remedy that.2016-03-07 02:23 PM
I am pretty sure it is dead. What i want to know is that it wont affect the rest of the GPIO Pins, right?
2016-03-07 03:38 PM
Well it is hard to know how localized the damage will be, or what the latent effects might be. You'd have to understand the structures involved, and the conduction path.
I'd assume this is just a scratch device you are testing/evaluating, so you could continue testing with other pins.2016-03-08 03:43 AM