cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F407VGT-DISCOVERY Cirrus 43L22 year 2016 HAL library incomplete?

zootroop
Associate II
Posted on March 18, 2016 at 00:59

Hi Everyone,

Simple question:

Is the STM32F407VGT-DISCOVERY Cirrus 43L22 HAL library released incomplete?

In the HAL library source and header files cs44l22.h and cs43l22.c I find the following obviously incomplete code!

Example:

/**

  * @brief Sets new frequency.

  * @param DeviceAddr: Device address on communication Bus.   

  * @param AudioFreq: Audio frequency used to play the audio stream.

  * @retval 0 if correct communication, else wrong communication

  */

uint32_t cs43l22_SetFrequency(uint16_t DeviceAddr, uint32_t AudioFreq)

{

  return 0;

}

Nothing is obviously happening in the code above so why is it there?

Another one here:

/**

  * @brief Start the audio Codec play feature.

  * @note For this codec no Play options are required.

  * @param DeviceAddr: Device address on communication Bus.   

  * @retval 0 if correct communication, else wrong communication

  */

uint32_t cs43l22_Play(uint16_t DeviceAddr, uint16_t* pBuffer, uint16_t Size)

{

  uint32_t counter = 0;

  

  if(Is_cs43l22_Stop == 1)

  {

    /* Enable the digital soft ramp */

    counter += CODEC_IO_Write(DeviceAddr, CS43L22_REG_MISC_CTL, 0x06);

  

    /* Enable Output device */  

    counter += cs43l22_SetMute(DeviceAddr, AUDIO_MUTE_OFF);

    

    /* Power on the Codec */

    counter += CODEC_IO_Write(DeviceAddr, CS43L22_REG_POWER_CTL1, 0x9E);  

    Is_cs43l22_Stop = 0;

  }

  

  /* Return communication control value */

  return counter;  

}

In the above code the most important values pBuffer and Size are not used. How comes?

And a last one here:

/** @defgroup CS43L22_Function_Prototypes

  * @{

  */

static uint8_t CODEC_IO_Write(uint8_t Addr, uint8_t Reg, uint8_t Value);

/**

  * @}

  */ 

If anyone can tell me what the above function is doing I'd be most happy.

Thx for sharing the state of affairs.

Greets,

Ben

#cs44l22-stm32f4-stm32f4discovery
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Nesrine M_O
Lead II
Posted on March 23, 2016 at 11:04

Hi Ben,

I am checking this issue. Please be patient when I could get some updated info

-Syrine-
Nesrine M_O
Lead II
Posted on April 26, 2016 at 14:38

Hi Ben,

For compatibility purpose, the same template is used in all audio components drivers. In the file wm8994.c that you find in the package STM32CUBEL4 V1.4.0 for example, you will see that these functions are ''complete''.

-Syrine-