cancel
Showing results for 
Search instead for 
Did you mean: 

ADC and DMA transfers for STM32F3.

kvresto
Senior
Posted on April 26, 2016 at 05:17

 

Hi.

I’m trying to get the DMA to transfer 10 data bytes from the ADC to memory (STM32F3.

So far I can get this to work in ADCDMA circular mode, and this 10 sample conversion takes place continuously.

I actually want the ADC to do 10 conversions only, and the DMA to transfer these into a buffer, and then at some time latter in code, I want to be able to start this 10 sample conversion again.

I made some changes which at the moment have not worked. With my current configuration I can sample 10 times and fill the buffer, but I cannot restart the ADC+DMA to do it again.

Can anyone point me in the right direction. I have included what is my code.

Thanks

kvresto

DMA INT:

/* Enable DMA1 clock */

RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1,

ENABLE

);

DMA_InitTypeDef

DMA_InitStructure;

DMA_DeInit(DMA1_Channel1);

DMA_InitStructure.

DMA_PeripheralBaseAddr

= ADC_CDR_ADDRESS;

DMA_InitStructure.

DMA_MemoryBaseAddr

= (

uint32_t

)&ADCConvertedBuffer;

DMA_InitStructure.

DMA_DIR

= DMA_DIR_PeripheralSRC;

DMA_InitStructure.

DMA_BufferSize

= 10;

DMA_InitStructure.

DMA_PeripheralInc

= DMA_PeripheralInc_Disable;

DMA_InitStructure.

DMA_MemoryInc

= DMA_MemoryInc_Enable;

DMA_InitStructure.

DMA_PeripheralDataSize

= DMA_PeripheralDataSize_HalfWord;

DMA_InitStructure.

DMA_MemoryDataSize

= DMA_MemoryDataSize_HalfWord;

DMA_InitStructure.

DMA_Mode

= DMA_Mode_Normal; <

---------

DMA_Mode_Circular;

DMA_InitStructure.

DMA_Priority

= DMA_Priority_Medium;

DMA_InitStructure.

DMA_M2M

= DMA_M2M_Disable;

DMA_Init(DMA1_Channel1, &DMA_InitStructure);

DMA_Cmd(DMA1_Channel1,

ENABLE

);

ADC INIT below:

----------------------------------------------------------------------------------------------------------

ADC_InitTypeDef        ADC_InitStructure;

ADC_CommonInitTypeDef  ADC_CommonInitStructure;

RCC_ADCCLKConfig(RCC_ADC12PLLCLK_Div1);

RCC_AHBPeriphClockCmd(RCC_AHBPeriph_ADC12, ENABLE);

ADC_StructInit(&ADC_InitStructure); //Fills ADC_InitStruct with its default value.

ADC_VoltageRegulatorCmd(ADC1, ENABLE);

Delay(0x2FFFF);

ADC_SelectCalibrationMode(ADC1, ADC_CalibrationMode_Single);

ADC_StartCalibration(ADC1);

while(ADC_GetCalibrationStatus(ADC1) != RESET );

calibration_value_1 = ADC_GetCalibrationValue(ADC1);

ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent;

ADC_CommonInitStructure.ADC_Clock = ADC_Clock_AsynClkMode;

ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled;

ADC_CommonInitStructure.ADC_DMAMode = ADC_DMAMode_OneShot;

ADC_CommonInitStructure.ADC_TwoSamplingDelay = 0;

ADC_CommonInit(ADC1, &ADC_CommonInitStructure);

/* */

ADC_InitStructure.ADC_ContinuousConvMode = ADC_ContinuousConvMode_Enable;

ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;

ADC_InitStructure.ADC_ExternalTrigConvEvent = ADC_ExternalTrigConvEvent_0;

ADC_InitStructure.ADC_ExternalTrigEventEdge = ADC_ExternalTrigEventEdge_None;

ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;

ADC_InitStructure.ADC_OverrunMode = ADC_OverrunMode_Disable;

ADC_InitStructure.ADC_AutoInjMode = ADC_AutoInjec_Disable;

ADC_InitStructure.ADC_NbrOfRegChannel = 1;

ADC_Init(ADC1, &ADC_InitStructure);

ADC_RegularChannelConfig(ADC1, ADC_Channel_7, 1, ADC_SampleTime_7Cycles5);

ADC_DMAConfig(ADC1, ADC_DMAMode_OneShot);                 <------------------ ADC_DMAMode_Circular);

ADC_DMACmd(ADC1, ENABLE);

ADC_Cmd(ADC1, ENABLE);

while(!ADC_GetFlagStatus(ADC1, ADC_FLAG_RDY));

ADC_StartConversion(ADC1);

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Walid FTITI_O
Senior II
Posted on April 26, 2016 at 12:20

Hi k.kvresto,

You need to use a timer to trig the ADC and launch conversion and DMA transfer. ADC Dual/triple interleaved mode is suitable for you with Multimode DMA request .

I recommend the ''ADC_DualModeInterleaved'' example in

http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/LN1939/PF257901

(since you are using the standard peripheral library) at this path:

STM32F4xx_DSP_StdPeriph_Lib_V1.6.1\Project\STM32F4xx_StdPeriph_Examples\ADC\ADC_DualModeInterleaved

-Hannibal-

kvresto
Senior
Posted on April 26, 2016 at 13:56

ok ,thank you Hannibal.