2024-11-30 03:20 PM - edited 2024-12-01 08:36 AM
Sorry, can I use STM32F407VET and STM32F4 Discovery board in CUBE IDE version 1.17.0.
If so, tell me where I can find information on how to implement it.
I tried on STM32F404VET and when compiling, it says that it does not see the controller.Thank
Solved! Go to Solution.
2024-12-01 09:49 AM
You have to use a st-link to connect to the f407 board. Do you??
2024-11-30 03:22 PM
sorry
CUBE IDE version 1.16.0
2024-11-30 06:28 PM
STM32F407VET6
Should be able to build for the part# if you type it in properly
2024-12-01 08:40 AM
thanks, but what's the "part #", sorry
2024-12-01 09:04 AM
Sorry, and can I find a way to connect the above boards in some STM documentation.Thanks
2024-12-01 09:49 AM
You have to use a st-link to connect to the f407 board. Do you??
2024-12-01 05:01 PM
ok. i undertsend.generaly create .bin file in progect cubeide , and use him in st-link utility when conectet st-link v2 to board stm32f4 cross swdio and swclk pin's.
Thank