2019-05-13 5:50 AM
Hi,
I'm using two STM32F407 LQFP-144 in SPI communication , one Master and one slave
when power supply is connected and program is running and spi send & recieve is okay , we disconnect board ( wiring) and then connect again , face off over heating ic and stm32f407 completely unusable
I read about hot swaping in the web but i'm not very exprience in this topic
2019-05-13 6:12 AM
STM32 overheat is often a sign that maximum input voltage on some pin was exceeded and the IC damaged. Read the datasheet about maximum rating carefully and look at possible errorr cases with your board.