stm32f407 SPI problem.
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-08-04 12:54 AM
Posted on August 04, 2015 at 09:54
Hello. I'm using stm32f407 eval board.
I want to communicate with gyro sensor in the board via SPI.But I can't get any signal from SPI AFIO pins.Please tell me if you find any errors from my codes.// SPI1 SCK(PA5), SPI1 MOSI(PA7), SPI1 MISO(PA6)GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5 | GPIO_Pin_6| GPIO_Pin_7;GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;GPIO_InitStructure.GPIO_OType = GPIO_OType_OD ; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;GPIO_Init(GPIOA, &GPIO_InitStructure); GPIO_PinAFConfig(GPIOA, GPIO_PinSource5, GPIO_AF_SPI1);GPIO_PinAFConfig(GPIOA, GPIO_PinSource6, GPIO_AF_SPI1);GPIO_PinAFConfig(GPIOA, GPIO_PinSource7, GPIO_AF_SPI1); //Chip select for LIS302DL (PE3)GPIO_InitStructure.GPIO_Pin = GPIO_Pin_3;GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_Init(GPIOE, &GPIO_InitStructure);RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1, ENABLE);RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA |RCC_AHB1Periph_GPIOB |RCC_AHB1Periph_GPIOC|RCC_AHB1Periph_GPIOD |RCC_AHB1Periph_GPIOE,ENABLE);void SPI_Configuration(void){SPI_InitTypeDef SPI_WITHROBOT;SPI_WITHROBOT.SPI_Direction = SPI_Direction_2Lines_FullDuplex;SPI_WITHROBOT.SPI_Mode = SPI_Mode_Master;SPI_WITHROBOT.SPI_DataSize = SPI_DataSize_8b;SPI_WITHROBOT.SPI_CPOL = SPI_CPOL_High; //for stm32f407 eval boardSPI_WITHROBOT.SPI_CPHA = SPI_CPHA_2Edge; //for stm32f407 eval boardSPI_WITHROBOT.SPI_NSS = SPI_NSS_Soft;SPI_WITHROBOT.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_16; // smt32f407 eval board max : 10Mhz Baud RateSPI_WITHROBOT.SPI_FirstBit = SPI_FirstBit_MSB;SPI_WITHROBOT.SPI_CRCPolynomial = 7;SPI_Init(SPI1,&SPI_WITHROBOT);SPI_Cmd(SPI1,ENABLE);}int SPI1_Read(int address){int data;GPIOE->BSRRH = GPIO_Pin_3; //nss low while((SPI1->SR & SPI_I2S_FLAG_TXE) == RESET);SPI1->DR = (address|0x80);while((SPI1->SR & SPI_I2S_FLAG_TXE) == RESET); SPI1->DR = (0xFF);while((SPI1->SR & SPI_I2S_FLAG_RXNE) == RESET);data = SPI1->DR; while((SPI1->SR & SPI_I2S_FLAG_RXNE) == RESET);data = SPI1->DR; while((SPI1->SR & SPI_I2S_FLAG_TXE) == RESET);while((SPI1->SR & SPI_I2S_FLAG_BSY) == SET); GPIOE->BSRRL = GPIO_Pin_3; //nss highreturn data;}Thank you
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-08-04 2:11 AM
Posted on August 04, 2015 at 11:11
void SPI_FPGA_Init(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
SPI_InitTypeDef SPI_InitStructure;
RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI4, ENABLE);
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOE, ENABLE);
GPIO_PinAFConfig(GPIOE, GPIO_PinSource2, GPIO_AF_SPI4);
GPIO_PinAFConfig(GPIOE, GPIO_PinSource5, GPIO_AF_SPI4);
GPIO_PinAFConfig(GPIOE, GPIO_PinSource6, GPIO_AF_SPI4);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2|GPIO_Pin_5|GPIO_Pin_6;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_DOWN;
GPIO_Init(GPIOE, &GPIO_InitStructure);
SPI_I2S_DeInit(SPI4);
SPI_InitStructure.SPI_Mode = SPI_Mode_Master;
SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex;
SPI_InitStructure.SPI_DataSize = SPI_DataSize_16b;
SPI_InitStructure.SPI_CPOL = SPI_CPOL_Low;
SPI_InitStructure.SPI_CPHA = SPI_CPHA_1Edge;
SPI_InitStructure.SPI_NSS = SPI_NSS_Soft;
SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_2;
SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB;
SPI_InitStructure.SPI_CRCPolynomial = 7;
SPI_Init(SPI4, &SPI_InitStructure);
SPI_Cmd(SPI4, ENABLE);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0|GPIO_Pin_1;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_DOWN;
GPIO_Init(GPIOE, &GPIO_InitStructure);
GPIOE->BSRRL=GPIO_Pin_0|GPIO_Pin_1;
}
uint16_t f[3]={0,0,0};
void FPGA_Update(void)
{
GPIOE->BSRRH=GPIO_Pin_0; //CS LOW
while (SPI_I2S_GetFlagStatus(SPI4, SPI_I2S_FLAG_TXE) == RESET);
SPI_I2S_SendData(SPI4, 1);
while (SPI_I2S_GetFlagStatus(SPI4, SPI_I2S_FLAG_RXNE) == RESET);
f[0]=SPI_I2S_ReceiveData(SPI4);
while (SPI_I2S_GetFlagStatus(SPI4, SPI_I2S_FLAG_TXE) == RESET);
SPI_I2S_SendData(SPI4, 1);
while (SPI_I2S_GetFlagStatus(SPI4, SPI_I2S_FLAG_RXNE) == RESET);
f[1] = SPI_I2S_ReceiveData(SPI4);
while (SPI_I2S_GetFlagStatus(SPI4, SPI_I2S_FLAG_TXE) == RESET);
SPI_I2S_SendData(SPI4, 2);
while (SPI_I2S_GetFlagStatus(SPI4, SPI_I2S_FLAG_RXNE) == RESET);
f[2]=SPI_I2S_ReceiveData(SPI4);
GPIOE->BSRRL=GPIO_Pin_0; //CS HIGH
}
Just modify pin, port, and clock supply enable functions as well as SPI, and it should work with no problems