Skip to main content
michaelweilguni9
Visitor II
August 3, 2015
Question

STM32F3 as class-D modulator

  • August 3, 2015
  • 1 reply
  • 677 views
Posted on August 03, 2015 at 15:34

Hello!

I'm trying to use an STM32F3 to drive a gate driver for a class-D amplifier using sigma-delta modulation. Therefore I use the internal comparator to compare a reference signal with the actual integrated signal of the amplifier output. Depending on the comparator's output, the amplifier is switched on/off. Currently I'm using a timer interrupt at 1 MHz and check the comparator state within the interrupt routine. The routine is quite short but nonetheless the interrupt occurs quite often, limiting the capabilies of the µC.

A D-flipflop with the comparator output as input, clocked by a 1MHz timer would also work, but an external component is required.

Does anyone know another way to toggle an output depending on the comparator state with an update rate of 1 MHz?

Thanks!
    This topic has been closed for replies.

    1 reply

    jjonethal
    Associate II
    August 4, 2015
    Posted on August 04, 2015 at 07:21

    Try pulse density modulation (PDM) over SPI.

    You could also use DMA to reduce interrupt load. Only external components required are low pass filter and speaker. Rc filter might be omitted if noise band is much above passband of speaker.

    You only need the data out MOSI signal for this application. SPI clock should be above 1... 3 MHZ for good noise rejection. Add another high pass filter around 20 Hz for speaker protection recommended.

    Jjo