cancel
Showing results for 
Search instead for 
Did you mean: 

Stm32f407 hang up in system memory when debug

totti001
Associate II
Posted on January 19, 2015 at 20:00

Hello everybody!

I've a very strange error. I've running application for stm32f407. I can download the code and it's working well. But when I want to debug with CoIDE the code stopped at 1FFF39c4 so in the system memory. At this point I reset the debugger and the code stop at the main function. I don't know the problem.

Can anyobody help me?
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0