STM32F407 discovery card debug error, Core is held in reset
- March 1, 2024
- 7 replies
- 4976 views
Now, I was only using the stlink part of the card to program another stm32 microcontroller. While running it in debug mode, I cut off the power of the card and it remained in debug mode all the time, in a way that I cannot understand now, and a connection with the card cannot be established in the cube ide program or utulity, cubeprogrammer programs. I get the error that the card is kept in reset mode. When I feed the NRST pin with 3 volts, I get a short connection. I only reset that much chip, but I think the problem is only in the stlink part. Can anyone help? I hope the problem is understandable, I will add the errors as well.
The LD1 pin of the card is on green, in this case, the stlink is not recognized in the Cube IDE program, when I remove it and insert it again, the code is not thrown. After the lalin LD1 turns green and red, the steady green light, which is the reset mode, turns on.
The error I get when I try to connect to the utility program is as follows:Can not connect to target!
If you're trying to connect to an STM32W1xx device, please select Normal or HotPlug mode from Target->Settings menu.
If you're trying to connect to a low frequency application , please select a lower SWD Frequency mode from Target->Settings menu.
13:47:06 : Core is held in reset
13:47:19 : Can not connect to target!