STM32F407 connection to st-link v2. I have a digital board running code from the external rom that connects to a color LCD panel, switches, and an some switches.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-10-15 12:33 PM
getting Error(4) and Error(7) at various point's in the error logs. USB communication seems to be working and firmware upgrade worked. Logs attached any thoughts?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-10-15 12:55 PM
Don't fiddle with the GPIO or configurations used by the debugger interface.
Don't put the core into a low power state, or cause bus transactions (DMA, etc) which interfere with attempts to wrestle the core into a halted state.
Make sure the debugger can control the NRST pins.
If strapping BOOT0 High makes the problems go away, you're code is doing something unhelpful.
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
‎2018-10-18 4:37 PM
Thanks for looking at this. An excellent clue. Code is running from flash and also making it impossible to halt the core. I incorrectly though st-link would work with anything running from flash.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-10-18 4:46 PM
Running from FLASH should be viable. If the debugger successfully connects to ROM, then it points to something your code is doing to interfere with normal operation.
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
‎2018-10-18 7:46 PM
Interesting, it's a bunch of DSP code, but it uses GPIO pins a bunch. By running from flash I'm thinking external flash. Is there an app note or something that discusses st-link's architecture and signal needs more than the notes I found that discuss cables and LEDs? Thank's for looking at my simple questions.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-10-18 11:27 PM
Can't this be more result of a hardware problem, like ground loops thrrough the debug cable, inadequate ground/return, too long debug cable, mcu supply problem...?
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-10-19 10:55 AM
Super idea. Surprisingly though the little board is really clean for signal integrity stuff though. This time I'm running into my limited understanding of the st-link architecture and an inability to control software very much. The st-link isn't connecting to the target at all. Lately I'm thinking that I need to stop the software at a point when the core quite so JTAG can work. I'm attempting to connect the st-link/v2 to my slightly broken Open_Source software radio .
FL
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-10-20 2:46 AM
> the little board is really clean for signal integrity stuff
You have the STLink onboard?
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-10-20 1:50 PM
It isn't at that level of clean, but it is only connected through a 7 cm cable with ground on the cable to the board. "really clean" are famous last words, but I'm certain I'm more fundamentally messed up.
I probably need to get more basic stuff correct, like: target-settings, software's use of GPIO, and core activity. Do you know of a summary sheet for target settings that works for the STM32F407? I think I may have a way of fixing the GPIO and core activity issue. Thanks for looking at my probably simple issue.
FL
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-10-20 5:02 PM
I don't want to say powersupply
change the cable. change the JTAG dongle.. change computer... change the Ground Lead
dont change the power supply ( :( )
do you have cache turned on ?