2023-10-23 8:37 AM
Good morning everyone, after collecting some data and storing it in various buffers, I am trying to write them to the serial port for further processing. I am experiencing issues as I can see that something is being written to the serial port, but not all the samples in the buffer are being printed. Any suggestions?
while (1)
{
HAL_UART_Receive (&huart2, UART1_rxBuffer, 1, 5000); //receive and store string
if(UART1_rxBuffer[0] == 115){
HAL_UART_Transmit(&huart2, UART1_rxBuffer, 1, 100); //print received string
if(flag == 1){ //check add finished
for(c=0;c<ADC_BUF_SIZE/2;c++){
sprintf(str, "%hu",(uint16_t*)buf1[c]); // conversion in str of value
HAL_UART_Transmit(&huart2, (uint8_t*)str, strlen(str), HAL_MAX_DELAY);
HAL_Delay(10);
}
HAL_UART_Transmit(&huart2,(uint8_t *)space,strlen(space),10); // string = “— — — — ;”
UART1_rxBuffer[0]=0; // start flag clear
flag = 0; // conversion adc clear
}
}
}
2023-10-23 12:21 PM
i have already done it. The adc sample the signal that i need and after the buffer filling I need, it does not change buf1 and buf2. The problem remains for me to print the values to serial and then process them externally.
for(i=0;i<ADC_BUF_SIZE/2;i++)
{
buf1[i] = (uint16_t)(adcBuf[i]&0x0000FFFF);
buf2[i] = (uint16_t)(adcBuf[i]>>16);
}
}
2023-10-23 12:32 PM
> sprintf(str, "%hu",(uint16_t*)buf1[c]); // conversion in str of value
Did you fix the error on this line? Show the corrected code.
2023-10-23 12:37 PM
while (1)
{
HAL_UART_Receive (&huart2, UART1_rxBuffer, 1, 5000);
if(UART1_rxBuffer[0] == 115){
HAL_UART_Transmit(&huart2, UART1_rxBuffer, 1, 100);
if(flag == 1){
for(c=0;c<ADC_BUF_SIZE/2;c++){
sprintf(str, "%u\r\n",((uint16_t*)buf1)[c]); // conversion in str of value
HAL_UART_Transmit(&huart2, (uint8_t*)str, strlen(str), HAL_MAX_DELAY);
HAL_Delay(100);
}
HAL_UART_Transmit(&huart2,(uint8_t *)space,strlen(space),10);
UART1_rxBuffer[0]=0;
flag = 0;
}
}
2023-10-23 12:52 PM - edited 2023-10-23 12:53 PM
So show what is in buf1 array, and what you're seeing being printed. And what are you printing to?
2023-10-24 2:04 AM
2023-10-24 3:03 AM
So what interface are you using to communicate with uart2? I suspect that is your weak link.
I am using a STM32F407VG-Discovery, used your code and saved the same data that you've provided. When i press the letter 's', I am able to output all the data correctly.
2023-10-24 3:18 AM
I am using a TTL converter because via usb I cannot see the serial port. Is there some setting I'm missing?