2016-10-27 7:15 PM
Hi
I want to use the baud rate to 921600 in stm32f405vgt6.
Can I use 921600 in UART1 ~ 6?
And Is the error rate to zero?
Thank you.
2016-10-27 10:57 PM
you can set it hand.
Same as in terminal 1 b software. Have you tried it?2016-10-27 11:50 PM
> Can I use 921600 in UART1 ~ 6?
That of course depends on the respective APB clock, which in turn depends on AHB clock. > And Is the error rate to zero? If that's your priority, use a crystal frequency of which is multiple of 921600, e.g. 7.3728MHz. JW