I2C Busy error
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2016-10-27 11:52 PM
Hi everyone.
I use the STM32F29 and have a similiar problem with the I2C as the following User:
/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/STM32F103XX%20I2C%20Busy%20Flag%20after%20unsuccessful%20transfer&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=458
The i2C works but sometimes when i use ''HAL_I2C_Mem_Read'' there is a timeout error.
After this timeout often the I2C no longer works because of a busy error.
When i measure SDA und the SCL I see that SDA is low and SCL is always high without a clock.
Why this error hapens and what can i do?
In the link above the solution is to make a stop signal with following code when the I2C is busy:
SET_BIT(hi2c1.Instance->CR1, I2C_CR1_STOP);
I2C_WaitOnFlagUntilTimeout(&hi2c1, I2C_FLAG_BUSY, SET, 1000);
When i call that code the busy error persists.When i measure SDA und SCL at the Busy error and after that code there are different states.Sometimes SCL and SDA are still low. But sometimes after I have made a hardware reset and try to repeat it, SDA is low and SCL is high or they are both high.
zaehler =0;
do
{
while (HAL_I2C_GetState(&hi2c1) !=
HAL_I2C_STATE_READY);
test = HAL_I2C_Mem_Read(&hi2c1, panel_touch_adresse, adresse_anpassen(mxt_object_message_count_t44.start_address), I2C_MEMADD_SIZE_16BIT, (uint8_t *)buffer, mxt_object_message_count_t44.size_minus_one +1, 100);
if(test == HAL_ERROR)
{
HAL_GPIO_WritePin(GPIOG, GPIO_PIN_7, RESET);
HAL_Delay(1000);
}
if(test == HAL_BUSY)
{
HAL_GPIO_TogglePin(GPIOG, GPIO_PIN_10);
HAL_Delay(1000);
SET_BIT(hi2c1.Instance->CR1, I2C_CR1_STOP);
I2C_WaitOnFlagUntilTimeout(&hi2c1, I2C_FLAG_BUSY, SET, 1000,HAL_GetTick());
}
if(test == HAL_TIMEOUT)
{
HAL_GPIO_TogglePin(GPIOG, GPIO_PIN_12);
HAL_Delay(1000);
}
zaehler++;
if (zaehler >=2) test = HAL_OK;
}while(test !=
HAL_OK);
#i2c #error #busy- Labels:
-
I2C