Skip to main content
life758
Associate III
November 26, 2015
Question

stm32f401re nucleo: PLL configuration

  • November 26, 2015
  • 5 replies
  • 1318 views
Posted on November 26, 2015 at 13:54

Hello everybody!

I'm trying to configure the main PLL to generate the max clock frequency (84 MHz on this board), and I'm using the HSI as PLL source.

I made some test:

- test1: HCLK=70 MHz

M=16

N=140

P=2

AHB_PR=1

APB1_PR=2

APB2_PR=1

As soon as I set the PLL output as HCLK, the uC stops working.

I mean:

- no blinking led

- random value on general purpose register

I made some test:

- test2: HCLK=35 MHz

M=16

N=140

P=2

AHB_PR=2

APB1_PR=2

APB2_PR=1

The uC works normally.

I'm missing some configuration (i.e. ART?), or the problem is the HSI and his accuracy?

Could someone help me to figure it out? Thanks!

Regards
    This topic has been closed for replies.

    5 replies

    waclawek.jan
    Super User
    November 26, 2015
    Posted on November 26, 2015 at 14:17

    Set FLASH latency properly.

    JW
    Tesla DeLorean
    Guru
    November 26, 2015
    Posted on November 26, 2015 at 14:32

    You also seem to be running the VCO very slowly. Doesn't it specify 192 - 432 MHz

    For 84 MHz, ST runs the VCO/PLL at 336 MHz and divides that by 4 (N)

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    waclawek.jan
    Super User
    November 26, 2015
    Posted on November 26, 2015 at 14:51

    I did not check for 'F401 specifically, but doesn't the reviewed PLL range apply for them too?

    https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/DispForm.aspx?ID=59917

    JW

    life758
    life758Author
    Associate III
    November 26, 2015
    Posted on November 26, 2015 at 15:47

    Thanks both of you for your input!

    Regads

    life758
    life758Author
    Associate III
    November 26, 2015
    Posted on November 26, 2015 at 19:10

    From the RM i read this:

    1. Program the new number of wait states to the LATENCY bits in the FLASH_ACR

    register

    2. Check that the new number of wait states is taken into account to access the Flash

    memory by reading the FLASH_ACR register

    3. Modify the CPU clock source by writing the SW bits in the RCC_CFGR register

    4. If needed, modify the CPU clock prescaler by writing the HPRE bits in RCC_CFGR

    5. Check that the new CPU clock source or/and the new CPU clock prescaler value is/are

    taken into account by reading the clock source status (SWS bits) or/and the AHB

    prescaler value (HPRE bits), respectively, in the RCC_CFGR register

    To achieve point 2 and 5 I used the istruction DSB and ISB. Is it right, or I need to check the state of bits?

    ************************************************************************************************************

            ; Set PLL at 70 MHz and use his output as clock sys

            LDR     r0, =0x40023800         ; RCC

            

            ldr     r1, =0x27015410         ; M=16, N=336, P=4, Q=7, HSI source PLL

            str     r1, [r0, #0x4]             ; PLLCFGR

            

            ldr     r1, [r0]                        ; RCC_CR

            orr     r1, r1, #(1 << 24)         ; PLLON=1

            str     r1, [r0]

            

            ; wait states for FLASH

            

            ldr     r2, =0x40023C00         ; FLASH register

            ldr     r3, =0x302

            ldr     r1, [r2]                    ; FLASH_ACR

            orr     r1, r1, r3                      ; ICEN=1, PRFTEN=1, 2 WS= 60<HCLK<=84

                                            

            str     r1, [r2]

            DSB

            ISB

            

            ldr     r1, =0x1002                          

            str     r1, [r0, #0x8]          ; PLL as clock sys, AHB_PR=1, APB1_PR=2, APB2_PR=1

            DSB

            ISB

    ***********************************************************************************************************

    Regards