cancel
Showing results for 
Search instead for 
Did you mean: 

HardFault while implementing USB MSC device

bnp979
Associate III
Posted on January 24, 2015 at 11:33

Hi,

I used the CubeMX framework to implement a USB mass storage device for my STM32L1 device.

I see that the code is issuing a hard fault when the laptop connected to the device is reading sectors from the device during the enumeration process.

The ''Fault Reports'' window in my uVision debugger indicates a INVPC userfault, which I am guessing is the cause for the hard fault.

I tried to figure out the instruction causing the fault by following instructions in the related app note at http://www.keil.com/appnotes/files/apnt209.pdf. 

When I break execution in the HardFault exception handler, I see that value of LR is 0xffffffff, which means I need to retrieve the context for the exception causing code from the PSP. However, the value of PSP is 0. 

Can somebody explain why this may the case?

How can I then retrieve the address of the instruction causing the fault?

Also, are there any known issues with the Cube USB MSC code?

Thanks,

Ben

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
stm32cube-t
ST Employee
Posted on November 26, 2015 at 18:35

Dear user,

You need to adjust the heap of your project (0x400).

Best regards
Posted on November 26, 2015 at 18:53

I'd double check both the heap and stack sizes defined in the startup.s are adequate.

Note the thread was started 11 months ago.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..