2015-12-02 02:44 AM
Hello everybody,
I started to use the ADC and I'd like to use every features of this module.While I read the reference manual and the datasheets i didn't found anything about using two input channels in differential mode. Did I miss something?Regards2015-12-02 06:48 PM
I'm not sure where you got the thought the F4 supported a differential mode. May be you're thinking about the F3
As I recall the F401 is a feature limited part, with only a single ADC, less memory, speed, timers, etc.2015-12-03 06:42 AM
Thanks!