2016-01-04 1:50 PM
Dear Community
I tried CLIVE1‘ example (
/public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/STM32F4-Discovery%20USB%20Mass%20storage&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F¤tviews=9633
)to connect a SD card via STM32F407 eval board to USB. I ported the files into a KEIL project which was setup using the latest drivers provided by ST. I used following preprocessor symbols:
STM32F40_41xxx, HSE_VALUE=8000000, USE_STM32F4_DISCOVERY,USE_STDPERIPH_DRIVER, USE_USB_OTG_FS,USB_OTG_FS_CORE
I checked the CLOCK setting using MCO and a scope and found everything appeared to be clocked correctly. However (I expected something similar) the example does not work (I don’t see anything detected by the USB master PC).
I started with troubleshooting and ended up here:
int8_t STORAGE_Init (uint8_t lun)
which appears to be part of a state machine - however it seems to be not toggled and I don’t know why.While trialling and erroring I would be very happy if someone could support me by giving a hint were to start with troubleshooting e.g. something like a state machine diagram or a flow chart of what happens inside the example in general.
null2016-01-04 3:26 PM
to connect a SD card via STM32F407 eval board to USB
Ok, and is this the DISCO board, or something else you can be more specific about?2016-01-05 2:15 PM
Dear Clive,
thank you for responding. I double checked my eval board: it is the STM32F407 Discovery Board Vers. C (meaning it contains the LIS3DSH accelerometer).
In the meantime I followed the code until USB_OTG_BSP_Init(USB_OTG_CORE_HANDLE *pdev) – where the VBUS seems to be initialized. Due to my pre settings the section “USE_USB_OTG_FS� is called (which I double checked once). I doubt that it initializes the right pins since the datasheet of the evalboard states: PA9 VBUS_FS; PA10 OTG-FS- ID; PA11 PM and PA12 ID. However I checked the OTG_FS_IRQHandler(void) which is called after the USB is plugged into the receptacle. Here an gintr_status.d32 is read: 0x49 0x53 0x50 0x4C thus it looks like USB initialization worked well (I didn’t checked the other contents of gintr_status yet).
2016-01-11 1:32 PM
Hi Folks,
it might be that CLIVE made his demo- prog for another kind of stm32F407 eval board than the one I tried to use for evaluating the code. To use CLIVES’ example code together with the STM32F407 discovery board (version C) and a e.g. the KEIL eval compiler some changes are required:
For proper SDIO detection intead of PH13 e.g. PD2 can be used - the other PINS need to be manually connected with the SD_CARD slot.
To make sure the SDcard is detected properly a test routine might be usefull:
if(SD_Detect() == SD_PRESENT) {
STM_EVAL_LEDOn(LED4);
} else STM_EVAL_LEDOn(LED5);
To make the USB Interface work some changes of the low level initialization are required:
#ifdef USE_USB_OTG_FS
Lprint(''USE_USB_OTG_FS\0'');
RCC_AHB1PeriphClockCmd( RCC_AHB1Periph_GPIOA , ENABLE);
/* Configure SOF ID DM DP Pins
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8 |
GPIO_Pin_11 |
GPIO_Pin_12;
*/
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10 |
GPIO_Pin_11 |
GPIO_Pin_12;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; //100 MHz
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ;
GPIO_Init(GPIOA, &GPIO_InitStructure);
//GPIO_PinAFConfig(GPIOA,GPIO_PinSource8,GPIO_AF_OTG1_FS) ;
GPIO_PinAFConfig(GPIOA,GPIO_PinSource10,GPIO_AF_OTG1_FS) ;
GPIO_PinAFConfig(GPIOA,GPIO_PinSource11,GPIO_AF_OTG1_FS) ;
GPIO_PinAFConfig(GPIOA,GPIO_PinSource12,GPIO_AF_OTG1_FS) ;
//PA9 VBUS_FS ; PA10 OTG-FS- ID; PA11 PM and PA12 ID
/* Configure VBUS Pin */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN;
GPIO_InitStructure.GPIO_OType = GPIO_OType_OD;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ;
GPIO_Init(GPIOA, &GPIO_InitStructure);
/* Configure ID pin */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10;
GPIO_InitStructure.GPIO_OType = GPIO_OType_OD;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP ;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; // 100MHz
GPIO_Init(GPIOA, &GPIO_InitStructure);
GPIO_PinAFConfig(GPIOA,GPIO_PinSource10,GPIO_AF_OTG1_FS) ;
RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE);
RCC_AHB2PeriphClockCmd(RCC_AHB2Periph_OTG_FS, ENABLE) ;
Since the STM32F407 version C board has a quartz included the following predefines will do a god job:
STM32F40_41xxx, HSE_VALUE=8000000,USE_STM32F4_DISCOVERY,USE_STDPERIPH_DRIVER, USE_USB_OTG_FS,USB_OTG_FS_CORE
Hope this helps and thankyou CLIVE for charing your code with us.
2016-01-11 4:24 PM
The
break out board uses PB.15 (defined in stm32f4_discovery.h w/SDIO additions) For the originalhttps://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/DispForm.aspx?ID=2816
demo I used PC.02 (2012)2018-02-07 12:19 PM
,
,
Link to the wire-wrapped board
,We’re moving the ST Community to a new platform to give you a better and more reliable community experience.