2018-02-02 11:43 AM
I'm trying to configure timer 7 in one-shot mode on the STM32L431 and am having an issue with my timer IRQ triggering as soon as I enable the interrupt. It seems like its preloaded with the period value, however I have the Auto Preload Reload disabled. This only happens the first time I enable the function. After that the code works as expected with my below functions. I have two questions:
// Restart timer function
void timerStartAskTimeout(void)
{ HAL_TIM_Base_Stop_IT(&hTimAsk); __HAL_TIM_SET_COUNTER(&hTimAsk, 0); HAL_TIM_Base_Start_IT(&hTimAsk);}// Timer Initialization Function
void timerInitializeAsk(void){ TIM_MasterConfigTypeDef sMasterConfig; hTimAsk.Instance = TIM7; hTimAsk.Init.Prescaler = (SYS_CLOCK_HZ / 1000) - 1; /* 1000Hz (1ms) */ hTimAsk.Init.CounterMode = TIM_COUNTERMODE_UP; hTimAsk.Init.Period = 1000; /* 250ms */ hTimAsk.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE; if (HAL_TIM_Base_Init(&hTimAsk) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); } if (HAL_TIM_OnePulse_Init(&hTimAsk, TIM_OPMODE_SINGLE) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); } sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET; sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE; if (HAL_TIMEx_MasterConfigSynchronization(&hTimAsk, &sMasterConfig) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }}#stm32l4-hal-timerSolved! Go to Solution.
2018-02-02 12:25 PM
I guess for configuration of timer you use a Cube function which deliberately sets the Update event through TIMx_EGR (in order to make effective any prescaler change).
In other words, clear the update flag in TIMx_SR before you enable the timer (I don't Cube so don't know the incantation for that, sorry).
JW
2018-02-02 12:25 PM
I guess for configuration of timer you use a Cube function which deliberately sets the Update event through TIMx_EGR (in order to make effective any prescaler change).
In other words, clear the update flag in TIMx_SR before you enable the timer (I don't Cube so don't know the incantation for that, sorry).
JW
2018-02-02 12:49 PM
I would 2nd JW's suggestion. I think forcing an update during initialization is a safer way of doing things but needs to be better documented and understood by the programmer. It is typical to reset the flags during initialization to avoid jumping to the ISR right away.
BTW, with all this trouble, it may be worth it to just poke at the registers directly.
2018-02-07 11:25 AM
Thanks, that seems to have done the trick. For reference the below line will clear the update flag:
__HAL_TIM_CLEAR_IT(&hTimAsk ,TIM_IT_UPDATE);
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.