cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4 - trigger digital output based on ADC - minimizing delays

paul2
Senior
Posted on July 08, 2014 at 09:30

Hi,

I’m trying to minimize control loop delays. Based on a certain analog value (adjustable threshold) a digital output is triggered. Reading ADC values is done by using DMA, digital outputs are driven without DMA.

Results measured by scoop: minimum delay ~300 μs, variation ~90 μs (min

300 μs,

max

390 μs

)

Does anybody have some tips/tricks/best practices minimizing ADC-DO control loop delays?

Thanks.

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
chen
Associate II
Posted on July 08, 2014 at 10:26

Hi

''

I’m trying to minimize control loop delays. Based on a certain analog value (adjustable threshold) a digital output is triggered. Reading ADC values is done by using DMA, digital outputs are driven without DMA.

''

''

Does anybody have some tips/tricks/best practices minimizing ADC-DO control loop delays?

''

Not sure what you mean by 'ADC control loop' ??

Try looking at the 'Analogue Watchdog' feature of the ADC.

It is basically 2 threshold values which can trigger an IRQ

frankmeyer9
Associate II
Posted on July 08, 2014 at 11:21

Why not using a discrete comparator, or a stm32f3 with integrated comparators ?

That would remove much software-induced delays from the loop.

For better suggestions, you might perhaps reveal more details about your application.

Posted on July 08, 2014 at 13:22

A singular ADC value, how frequently? Perhaps you could avoid DMA, or use an alternate ADCx unit, and use the EOC interrupt to read/process the threshold

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..