stm32f4 to stm32f103
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2016-10-21 1:06 AM
Posted on October 21, 2016 at 10:06
i have stm32f407 discovery board and the stm32f407 is damage
but i have stm32f103vct6 100pin chip can i replace stm32f407 by stm32f103vct6 ????? i know there is pin different can i solve it ?
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2016-10-21 1:44 AM
Posted on October 21, 2016 at 10:44
Hello,
I recommend you to take a look to the Application note ''Migration of microcontroller applications from STM32F1 Series to STM32F4 Access lines''. This reference can help you to determine differences between the two series with give attention to pinout, peripherals and system clock...You can refer to the document under page, start from the template project in the package and then add your own update.The migration for the HAL library is easily from one device to another as functions' names are the same for all series.
Regards