STM32F4 slave uart DMA circular buffer
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-06-09 10:00 AM
I have to
write new driver for
uart
slave
interface
with
a
STM32F407
For RX I thought I
enable DMA
incircular
buffer
mode. The device is always ready to receive and with HC
and
TCDMA
interrupt I
can
download the RX data
from the receiver buffer.
But with message rx tail or if the length of the received message can't trigger a DMA interrupt how I can solve ?Someone
has already solved
a
similar
situation
Thanks #stm32-usart-dma- Labels:
-
UART-USART
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-06-09 12:02 PM
Your TX routine would have to use normal mode and describe linear regions of the ring buffer, and split the wrapping condition. If there is no data to send you'd simple need to poll the buffer occasionally (say 1 KHz task), and restart the next transaction.
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-06-09 12:31 PM
If the incoming message is variable length then you need a method to detect an idle period after the last character is received. ST recommends using a timer attached to the RX incoming bit stream. Set up the time to reset on every edge change, with a timeout period sufficient to guarantee an end of message idle period.
As long as incoming data arrives the timer is constantly being reset, meaning the RX line is active and DMA is storing data. When the incoming data stops, there are no bit transitions and eventually the timer overflows, signaling an idle period. Once the timer overflows you can stop the DMA and process the data in the buffer. I use this on a high speed (460Kbaud) RS-485 serial line, USART1 along with timer TIM9, the TIM9 CH1 input connected to USART1 RX input pin. I set the TIM9 to reset on capture, with a timeout based on selected baud rate. Be sure to use a timer that can reset on capture input pin, not all have this capability. I use Modbus as the line protocol, which defines an inter-message gap time. The timeout is determined by the baud rate, with a minimum time, as defined in the Modbus standard. With a time gap you don't have to detect framing characters for the message. Jack Peacock- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-06-09 2:26 PM
thanks for the
quick
answers
The idea of
​​polling
the
buffer
seems to be the
easiest
.going
even
at high speeds
eg
.460kbps
every 1ms
I receive46bytes
with
128 or 256 bytes
buffer
should
be safe enough
to be able to
flush the buffer
before
DMA write overflow at 1ms sampling rate
In fact even
I was thinking
to the Jack solution
My idea was
to
trigger
the timer
with
RXNE
interrupt
but the documentation
warns that
if you use the
DMA
is not possible to
activate
the
interrupt
RXNEIE
(
sich!
)Jack describe a good solution
but I must
change the
hw
...
I have to think
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-06-17 8:21 AM
I went on an even simpler route by using just the ''plain old'' DMA to transfer the RX data into a circular buffer without any interrupts. With the higher speeds (several MBd) this seems to be the only alternative.
There is no generic way to detemine the buffer size. Obviously it has to be large enough to tolerate the burst loads. If a rapid response to short UART messages is required, a time based polling, such as 1 ms or 10 ms, can be used to determine if enough data has been received. The usage of the NDTR register is essential in that routine. You can find more details in a tutorial I have written about this subject athttp://www.emblocks.org/wiki/tutorials/f401_f429_disco/serial
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-12-10 3:17 PM