STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L476 ClockDivision

Posted on August 25, 2016 at 09:59 Hello, I am using the board Nucleo-L476RG, the system core clock is running at 80 Mhz. I don't understand what is the purpose of ClockDivision. I thought that I can divide the frequency by 4 if I setTIM_CLOC...

How to add user source files to STM32CubeMX project?

Posted on August 23, 2016 at 19:58I created a project with STM32CubeMX, generated the source code (for MDK-ARM5), then expanded my code by adding a couple of new source files.Later, I went back to tweak my original Cube project and when I regenerate...

st32F I/O protection circuit

Posted on August 25, 2016 at 07:42Hello everyone, i have a st32F407 and i was thinking if it is working on 3.3V and almost all its pins are 5V tolarant what kind of protection circuit it has for overvoltage and ESD. I saw on the reference manual in ...

td by Associate II
  • 1966 Views
  • 3 replies
  • 0 kudos

Problem with arm_math.h in the newest mxCube

Posted on July 15, 2016 at 12:35 Hello there, I have just updated mxCube to version 4.0. I am genereting startup code for SW4STM I am using arm_math libarry. Since this version, I am getting warning I should not be getting... For example: ...

STM32f103 Counter (EXTI/Timer)

Posted on August 04, 2016 at 20:09 Hi there. i want to make a pulse counter with stm32f103RB. at first time i using EXTI to count the pulses means configure one of EXTI in falling or rising edge and in the IRQ_hander routine increase a var...

amir_lm35 by Associate II
  • 5824 Views
  • 10 replies
  • 0 kudos

STM32FO30R8T6 TIM1

Posted on August 22, 2016 at 16:25Hi,i have a question about Timer1 of the �C mentioned above.I want to use the Timer1 for a SW-Timer with second-resolution.I have the idea, to start the timer with a frequency of 1 KHz and use the Auto-repition-Coun...

ali23 by Associate
  • 1941 Views
  • 4 replies
  • 0 kudos

Problem in six-step PWM generatioin

Posted on August 23, 2016 at 04:36I am using STM32F3 Discovery board to generate six-step PWM signals for BLDC motor drive. The switching was done in SysTick ISR by generating a SW COMG event. When I checked the PWM output on oscilloscope, however, ...

song by Associate II
  • 2172 Views
  • 4 replies
  • 0 kudos