cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4 LTDC - scan lines

prog
Associate
Posted on July 29, 2016 at 13:19

Hi All,

My hardware is custom STM32F429 board with 7'' TFT.

Display has no U/D or R/L display mode select pin.

I don't see datasheet LTDC registers to configure scanning order.

Actually i do it manually in software, perhaps using DMA2D will be quicker but still is to slowly

There is some idea to setup it ?

Andrew

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
slimen
Senior
Posted on July 29, 2016 at 14:52

Hi,

You can have a look to the LTDC examples under STM32CubeF4 package, it maybe helpful for you:

STM32Cube_FW_F4_V1.13.0\Projects\STM324x9I_EVAL\Examples\LTDC\LTDC_Display_2Layers

This example can be a starting point to learn about programming the display as it describes how to configure the LTDC peripheral to display two Layers at the same time. 

You can also, refer to the 

http://www.st.com/content/ccc/resource/technical/document/reference_manual/3d/6d/5a/66/b4/99/40/d4/DM00031020.pdf/files/DM00031020.pdf/jcr:content/translations/en.DM00031020.pdf

, section 16 LCD-TFT controller (LTDC)

Regards