2015-04-13 2:22 PM
I'm working on a very space-constrained design for an STM32F405RGT6 that needs 48MHz for USB FS. Ideally the crystal is a 3.2mm x 2.5mm footprint. Availability suggests that 12MHz is a perfect HSE for my needs. I've worked out all of the PLL values so I can achieve a full 168MHz SYSCLK and 48MHz USB with a 12MHz HSE so all looks OK there.
I'm reading over AN2867 (Oscillator Design Guide for STM32) but honestly, almost all of the requirements are over my head as a software type. My first crystal selection was an 8MHz with an ESR of 500 ohms. Problems galore...The system mostly ran fine and the HSE RDY register seemed to set fine but DFU flat didn't work and USB was beyond flaky. Removing my crystal and using the 8MHz HSE/MCO from a STM32F4 Discovery board into my custom PCB for clock made everything work great so I know I just have to rework the HSE design.NDK NX3225SA
Frequency: 12MHzStability: +/- 25ppmTolerance: +/- 15ppmLoad Capacitance: 8pFLevel of Drive: 10uW (Max 200 uW)ESR: 100 OhmDigikey:http://www.digikey.com/product-detail/en/NX3225SA-12MHZ-STD-CSR-6/644-1180-1-ND/3125569Datasheet:http://www.ndk.com/images/products/catalog/c_NX3225SA-STD-CSR-6_e.pdfI think that's the best 12MHz crystal I can find for the F4 in a 3.2 x 2.5 footprint but I'm really not sure I'm looking at everything right and I don't understand how to calculate the ''ratio'' that they're talking about. I hate to wait for another PCB with this footprint just to find it won't work.Any help is appreciated!2015-04-18 8:30 AM
Anybody? I'm essentially just trying to figure out which values to use to calculate the same thing discussed in the post linked below. It seems to be critical for me to figure out.
https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=https%3a%2f%2fmy%2est%2ecom%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fcortex_mx_stm32%2fCrystal%20drive%20level&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tvi...2016-04-14 3:58 AM
Hi Mr. Blinky,
You can refer to
http://www.st.com/web/en/resource/technical/document/application_note/CD00221665.pdf
Oscillator design guide for ST microcontrollers.-Hannibal-
Anybody? I'm essentially just trying to figure out which values to use to calculate the same thing discussed in the post linked below. It seems to be critical for me to figure out.
https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=https%3a%2f%2fmy%2est%2ecom%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fcortex_mx_stm32%2fCrystal%20drive%20level&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tvi...2016-04-14 6:52 AM
Hi Mr. Blinky,
Here is a spreadsheet that I use to implement the equations from the design guide. To the best of my knowledge it is correct (gives the same answer as the example in the design guide). ________________ Attachments : Discovery_Crystal_Calculator.xlsx : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0mW&d=%2Fa%2F0X0000000bdZ%2FysamJqsnSSD6BMl0KRfh6lCgiUwjCkmZmLaGwApGZJc&asPdf=false