cancel
Showing results for 
Search instead for 
Did you mean: 

SDRAM on STM32F429I with disabled 16-bit byte

smrtkai
Senior
Posted on April 13, 2016 at 12:37

Hi,

I am using a STM32F429I discovery board. I have a running project in which I can generate code from STM32CubeMX. I would like to disable ''16-bit byte'', because I need the pin PE0 as a clock source for TIM4 (ETR2).

The FMC controller for SDRAM2 is configured as follows:

Clock and chip enable: SDCKE1+SDNE

Internal bank numer: 4 banks

Address: 13 bits

Data: 16 bits

16-bit byte enable

Does anyone knows if this is possible?
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
slimen
Senior
Posted on April 14, 2016 at 14:22

Hello,

Using CubeMX, it's possible to disable ''16-bit byte'' and enable the pin PE0 as a clock source for TIM4 (ETR2).

I hope that answer your question, else you can provide more information about your issue.

Regards

-ForumSTM32-
scott23
Associate II
Amel NASRI
ST Employee
Posted on April 14, 2016 at 15:23

Hi jisa.sana,

The provided link is out of topic I think.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.