cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f4 discovery st-link usb problem

jbl_raw
Associate II
Posted on May 30, 2013 at 00:14

i have problem with st link swd in discovery board.

the usb device have problem in this picture. i think it need usb driver for discovery baord.

0690X00000605PpQAI.png

4 REPLIES 4
Posted on May 30, 2013 at 01:22

i think it need usb driver for discovery baord.

Ok, so could you not locate one via a simple Google or Bing search?

Or in a tool chain directory like \Keil\ARM\STLink which has drivers and firmware updates.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
jbl_raw
Associate II
Posted on May 31, 2013 at 19:20

thank you. problem is solved.

it was need to search to found new hardware after st link driver setup

mmensch
Associate II
Posted on July 30, 2013 at 10:35

Thanks Ahmed, that helped me too.

To give some more info to people with that problem:

You need to plug in the ST-Link (in my case it is an STM32F0 Discovery board), then go to Device Manager (the picture above) - Action - Search for new hardware (or so, I translated this from my windows version). The rest runs automatically.

Maybe the problem results from first plugging in the ST Link (which leads to a failed driver install by windows) and the installing the driver with the file st-link_v2_usbdriver.exe, so maybe there is no problem when you first install the driver.

Thanks again

Martin

069349773
Associate II
Posted on July 30, 2013 at 11:18

I first installed the driver, rebooted PC, and only then put the usb cable, and it works )))