STM32F4 Discovery. CAN communication FAIL. HAL_TIMEOUT.
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-09-22 6:09 AM
Posted on September 22, 2015 at 15:09
Hello everyone, this is my first post in the forum, but I read a great deal of threads about CAN communication between PC and STM32 Discovery using HAL Libraries.
The problem, basically, is that I'm unable to send/receive CAN frames. The configuration of the peripheral is pretty standard, and my code looks right, but when I try to send a message through HAL_CAN_Transmit I get an HAL_TIMEOUT state.Can someone help me? I'm pretty stuck!CAN_HandleTypeDef CAN_HandleStruc;void CAN1_Init(){ //Struct for GPIO and CAN initialization GPIO_InitTypeDef GPIO_InitStruc; CAN_FilterConfTypeDef CAN_FilterConfStruc; static CanRxMsgTypeDef msgRX; static CanTxMsgTypeDef msgTX; //Enable GPIOD clock __HAL_RCC_CAN1_CLK_ENABLE(); __GPIOD_CLK_ENABLE(); GPIO_InitStruc.Pin = CAN_RX_PIN | CAN_TX_PIN; GPIO_InitStruc.Mode = GPIO_MODE_AF_PP; GPIO_InitStruc.Speed = GPIO_SPEED_HIGH; //100 Mhz GPIO_InitStruc.Pull = GPIO_PULLUP; GPIO_InitStruc.Alternate = GPIO_AF9_CAN1; HAL_GPIO_Init(CAN_GPIO_PORT,&GPIO_InitStruc); /*♯&sharp1 Configure the CAN peripheral ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/ // CAN Baudrate (1Mbps) = 168MHz/[(SJW+BS1+BS2)*Prescaler] HAL_CAN_DeInit(&CAN_HandleStruc); CAN_HandleStruc.Instance = CAN1; CAN_HandleStruc.pTxMsg = &msgTX; CAN_HandleStruc.pRxMsg = &msgRX; CAN_HandleStruc.Init.TTCM = DISABLE; CAN_HandleStruc.Init.ABOM = DISABLE; CAN_HandleStruc.Init.AWUM = DISABLE; CAN_HandleStruc.Init.NART = DISABLE; CAN_HandleStruc.Init.RFLM = DISABLE; CAN_HandleStruc.Init.TXFP = DISABLE; CAN_HandleStruc.Init.Mode = CAN_MODE_NORMAL; CAN_HandleStruc.Init.SJW = CAN_SJW_1TQ; CAN_HandleStruc.Init.BS1 = CAN_BS1_14TQ; CAN_HandleStruc.Init.BS2 = CAN_BS2_6TQ; CAN_HandleStruc.Init.Prescaler = 8; if(HAL_CAN_Init(&CAN_HandleStruc) != HAL_OK) Error_Handler(); /*♯&sharp2 Configure the CAN filter ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/ CAN_FilterConfStruc.FilterNumber = 0; CAN_FilterConfStruc.FilterMode = CAN_FILTERMODE_IDMASK; CAN_FilterConfStruc.FilterScale = CAN_FILTERSCALE_32BIT; CAN_FilterConfStruc.FilterIdHigh = 0x0000; CAN_FilterConfStruc.FilterIdLow = 0x0000; CAN_FilterConfStruc.FilterMaskIdHigh = 0x0000; CAN_FilterConfStruc.FilterMaskIdLow = 0x0000; CAN_FilterConfStruc.FilterFIFOAssignment = CAN_FILTER_FIFO0; CAN_FilterConfStruc.FilterActivation = ENABLE; //CAN_FilterConfStruc.BankNumber = 14; HAL_CAN_ConfigFilter(&CAN_HandleStruc,&CAN_FilterConfStruc); //Enable CAN1 RX Interrupt HAL_NVIC_SetPriority(CAN1_RX0_IRQn,0,0); //Priority and Sub Priority HAL_NVIC_EnableIRQ(CAN1_RX0_IRQn); //Enable FIFO0 pending interrupt __HAL_CAN_ENABLE_IT(&CAN_HandleStruc,CAN_IT_FMP0); /*♯&sharp3 Configure Transmission process ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/ CAN_HandleStruc.pTxMsg->StdId = 0x1; CAN_HandleStruc.pTxMsg->ExtId = 0x0; CAN_HandleStruc.pTxMsg->RTR = CAN_RTR_DATA; CAN_HandleStruc.pTxMsg->IDE = CAN_ID_STD; CAN_HandleStruc.pTxMsg->DLC = 2; CAN_HandleStruc.pTxMsg->Data[0] = 0x01; CAN_HandleStruc.pTxMsg->Data[1] = 0x01; //Below the function that return an HAL_TIMEOUT!!!!!! HAL_CAN_Transmit(&CAN_HandleStruc, 10); }I should write down the RX interrupt, but meanwhile I'm trying to get Polling mode working..with no result so far. #can #stm32f4-discovery
Labels:
- Labels:
-
CAN
-
STM32F4 Series
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-09-22 1:59 PM
Posted on September 22, 2015 at 22:59
The CAN ESR register should give you some hint as to what is wrong. Do you get any kind of error on the other CAN node?
Jack Peacock