2011-12-22 2:09 PM
I have built a baseboard for the STM32F4 Discovery module. It has two RS232 ports and two 50-pin headers allow easier connection to the other pins.
I have some photos on my blog:http://kornakprotoblog.blogspot.com/2011/12/breakout-board-for-stm32f4-discovery.html
It uses a BusBoard-3U proto board to connect the DIL headers pin-to-pin. A parts list is provided. My first project is to use it to interface to a GPS module. I would appreciate any feedback anyone has on what they would like to see on more sophisticated breakout boards. Please post here, or you can email me at kornak.busboard@gmail.com with any comments, suggestions, or specific questions. Thanks! Scot Kornak #stm32f4 #stm32f4-discovery