2011-11-15 5:41 AM
I have been able to successfully setup the ADC3 to set the SR, AWD flag when an input exceeds my threshold set. What I am now looking to do is put the processor in sleep mode (via __WFI();) and then have it wake up via the AWD interrupt.
Here is my ADC setup:/* Configure ADC3 Channel12 pin as analog input ******************************/
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ; GPIO_Init(GPIOC, &GPIO_InitStructure); /* ADC Common Init **********************************************************/ ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent; ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div2; ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled; ADC_CommonInitStructure.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_5Cycles; ADC_CommonInit(&ADC_CommonInitStructure); /* ADC3 Init ****************************************************************/ ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b; ADC_InitStructure.ADC_ScanConvMode = DISABLE; ADC_InitStructure.ADC_ContinuousConvMode = ENABLE; ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None; ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right; ADC_InitStructure.ADC_NbrOfConversion = 1; ADC_Init(ADC3, &ADC_InitStructure); /* ADC3 regular channel12 configuration *************************************/ ADC_RegularChannelConfig(ADC3, ADC_Channel_12, 1, ADC_SampleTime_3Cycles); /* Enable DMA request after last transfer (Single-ADC mode) */ ADC_DMARequestAfterLastTransferCmd(ADC3, ENABLE); ADC_AnalogWatchdogThresholdsConfig(ADC3, 0x300, 0x0); ADC_AnalogWatchdogSingleChannelConfig(ADC3, ADC_Channel_12); ADC_ClearFlag(ADC3, ADC_FLAG_AWD); ADC_AnalogWatchdogCmd(ADC3, ADC_AnalogWatchdog_SingleRegEnable); ADC_ITConfig(ADC3, ADC_IT_AWD, ENABLE); // Enable ADC1 AWD interruptI then configure the NVIC register as follows:NVIC_InitTypeDef NVIC_InitStructure;
/* Configure and enable ADC interrupt */ NVIC_InitStructure.NVIC_IRQChannel = ADC_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure);When the AWD threshold is met, the processor never wakes up (regardless of ADC input). I'm thinking I don't have an IRQ registered correctly, or I need to setup an IRQ Handler, but I'm not sure where to look for this. Please advise, and thanks.2011-11-17 8:32 PM
WFI is Wait For Interrupt. Thus you have to interrupt. If you interrupt and don’t provide an ISR you will go to never land. I would first put a breakpoint on the trap handler. If it goes off you have your answer. If not write a dummy handler, put a breakpoint on it and try to understand why no interrupt.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.