2013-06-13 2:08 AM
hi,
I am working on a project where I need to sample some data using the ADC in discovery at 1MSPs and transfer it to a raspberry pi board via SPI. As Rpi supports only SPI master mode the discovery board acts as a slave.However I am not able to get the discovery board work in slave mode. I am posting it a sample program I used to test spi in discovery board . &sharpinclude <stm32f4xx.h>&sharpinclude <stm32f4xx_spi.h>uint8_t SPI1_send(uint8_t data);// this function initializes the SPI1 peripheralvoid init_SPI1(void){ GPIO_InitTypeDef GPIO_InitStruct; SPI_InitTypeDef SPI_InitStruct; // enable clock for used IO pins RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE); /* configure pins used by SPI1 * PA5 = SCK * PA6 = MISO * PA7 = MOSI */ GPIO_InitStruct.GPIO_Pin = GPIO_Pin_13 | GPIO_Pin_14 | GPIO_Pin_15; GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStruct.GPIO_OType = GPIO_OType_PP; GPIO_InitStruct.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOB, &GPIO_InitStruct); // connect SPI1 pins to SPI alternate function GPIO_PinAFConfig(GPIOB, GPIO_PinSource13, GPIO_AF_SPI2); GPIO_PinAFConfig(GPIOB, GPIO_PinSource14, GPIO_AF_SPI2); GPIO_PinAFConfig(GPIOB, GPIO_PinSource15, GPIO_AF_SPI2); // enable clock for used IO pins RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOE, ENABLE); // enable peripheral clock RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI2, ENABLE); /* configure SPI1 in Mode 0 * CPOL = 0 --> clock is low when idle * CPHA = 0 --> data is sampled at the first edge */ SPI_InitStruct.SPI_Direction = SPI_Direction_2Lines_FullDuplex; // set to full duplex mode, seperate MOSI and MISO lines SPI_InitStruct.SPI_Mode = SPI_Mode_Slave; SPI_InitStruct.SPI_DataSize = SPI_DataSize_8b; // one packet of data is 8 bits wide SPI_InitStruct.SPI_CPOL = SPI_CPOL_Low; // clock is low when idle SPI_InitStruct.SPI_CPHA = SPI_CPHA_1Edge; // data sampled at first edge SPI_InitStruct.SPI_NSS = SPI_NSS_Soft | SPI_NSSInternalSoft_Set; // set the NSS management to internal and pull internal NSS high SPI_InitStruct.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_2; // SPI frequency is APB2 frequency / 4 SPI_InitStruct.SPI_FirstBit = SPI_FirstBit_MSB;// data is transmitted MSB first SPI_Init(SPI2, &SPI_InitStruct); SPI_Cmd(SPI2, ENABLE); // enable SPI1}/* This funtion is used to transmit and receive data * with SPI1 * data --> data to be transmitted * returns received value */uint8_t SPI2_recv(){ uint8_t temp ; while( !(SPI2->SR & SPI_I2S_FLAG_RXNE) ); // wait until receive complete temp = SPI2->DR ; // write data to be transmitted to the SPI data register while( !(SPI2->SR & SPI_I2S_FLAG_TXE) ); // wait until transmit complete while( SPI2->SR & SPI_I2S_FLAG_BSY ); // wait until SPI is not busy anymore return temp; // return received data from SPI data register}&sharpif 1int main(void){ uint8_t received_val = 0; init_SPI1(); while(1){ received_val = SPI2_recv(); // transmit dummy byte and receive data }}&sharpendifWhen I debug the code I see that while( !(SPI2->SR & SPI_I2S_FLAG_RXNE) ); condition is never being met. Also how to I enable interrupts for the same? #slave #discovery #stm32f4 #spi2013-08-03 7:14 AM
2013-12-10 12:15 AM
Hello, I am trying to solve a similar problem. I have problem with that while loop too and I will try to solve the problem with interrupts. Did you solve your problem and if so how did you use interrupts?