cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4-DIS, camera 5mp, DCMI interface

aamzil.ilyas9
Associate II
Posted on July 19, 2016 at 17:32

Hi,I'am starting a new project and I will need to interface the STM32F4-discovery with a camera ( 5mp ),can you suggest me a DCMI camera module with 5mp resolution

4 REPLIES 4
Posted on July 20, 2016 at 02:55

Not sure it supports that resolution. You definitely don't have enough memory to manage such an image.

Consider an F7 board with SDRAM, and a DCMI connector...

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
aamzil.ilyas9
Associate II
Posted on July 22, 2016 at 14:29

Thank you clive1 for your answer, but if i configure the camera output format to GRB 4:2:2 ( it must give compressed frames) it will work? 

Thank you in advance

aamzil.ilyas9
Associate II
Posted on August 01, 2016 at 21:50

help me please

Posted on August 01, 2016 at 22:10

Not sure there is a great deal of help to be had here. Have you discussed this with your project supervisor?

Have you experimented with the regular STM32F4-CAM module to get comfortable with that, and the provided software? Have you reviewed the Reference Manual for the STM32F4 DCMI unit, and the DMA unit?

What processing do you plan on doing with the image?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..