cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4 clock configuration Excel tool only permits up to 25MHz HSE clock

szbrozek9
Associate II
Posted on September 12, 2012 at 21:43

According to the datasheet, the STM32F4 processors can accept up to 50MHz on the external clock input, but the clock configuration tool only permits inputs up to 25MHz. Is this intentional? Does that mean there's some caveat to higher input clocks that I don't know about?

Thanks for the insight!

-Sasha
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on September 12, 2012 at 22:44

Does that mean there's some caveat to higher input clocks that I don't know about?

I think it means the crystal oscillator circuit is rated from 4-26 MHz (or 4-16 if you look at the block diagram). So the ability of OSC_IN/OSC_OUT to sustain a stable oscillation in a suitable crystal, and circuit configuration.

They specify an external clock (OSC_IN Only) from 1-50 MHz ''By Design, Not tested in production''

The PLL needs to be clocked in the 1-2 MHz range for it's comparison frequency (PLL_M, valid range 2-63)

You need to use the HSEBYP and HSEON bits in the RCC_CR to use an EXTERNAL source, ie it turns OFF the OSC_OUT driver

AHB must be at least 25 MHz for Ethernet operation.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..