2016-10-26 9:28 PM
Hello
I am using stm32f373 chip to implement SDADC, USART, Timer, etc, and now I have a problem with interrupt.
I tested USART1 interrupt code as below. If I send any character to STM, then it would receive it and send back to my computer. But I couldn't receive anything.
void USART1_IRQHandler(void)
{ char receive_data; if(USART_GetITStatus(USART1, USART_IT_RXNE) != RESET) { receive_data = USART_ReceiveData(USART1) & 0xFF; USART_SendData(USART1, receive_data); while(USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET ); USART_ClearITPendingBit(USART1, USART_IT_RXNE); } }void usart1_test_interrupt(void)
{ GPIO_InitTypeDef GPIO_InitStructure; USART_InitTypeDef USART_InitStructure; NVIC_InitTypeDef NVIC_InitStructure;/* AHB Clock enable for USART(GPIOA9, A10) */
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE); /* USART1 clock enable */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE); /* USART1 Pins configuration **************************************************/ GPIO_DeInit(GPIOA); /* Connect pin to Periph */ GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_7); GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_7); /* Configure pins as AF pushpull */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9 | GPIO_Pin_10; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOA, &GPIO_InitStructure);/* USARTx configured as follow:
- BaudRate = 115200 baud - Word Length = 8 Bits - Stop Bit = 1 Stop Bit - Parity = No Parity - Hardware flow control disabled (RTS and CTS signals) - Receive and transmit enabled */ USART_DeInit(USART1); USART_InitStructure.USART_BaudRate = 115200; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_Init(USART1, &USART_InitStructure); /* Enable the USART1 */ USART_Cmd(USART1, ENABLE); USART_ITConfig(USART1, USART_IT_RXNE, ENABLE); /* Configure one bit for preemption priority */ //NVIC_PriorityGroupConfig(NVIC_PriorityGroup_1); /* Enable the USART1 Interrupt */ NVIC_InitStructure.NVIC_IRQChannel = USART1_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); /* Enable the USART1 */ USART_Cmd(USART1, ENABLE); }Now I tested USART1 polling code as below which implement just same thing but using polling method instead of using interrupt method. Then it works!
void usart1_test_polling(void)
{ GPIO_InitTypeDef GPIO_InitStructure; USART_InitTypeDef USART_InitStructure; char receive_data;/* AHB Clock enable for USART(GPIOA9, A10) */
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE); /* USART1 clock enable */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE);/* USART1 Pins configuration **************************************************/ GPIO_DeInit(GPIOA); /* Connect pin to Periph */ GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_7); GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_7); /* Configure pins as AF pushpull */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9 | GPIO_Pin_10; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOA, &GPIO_InitStructure);
/* USARTx configured as follow:
- BaudRate = 115200 baud - Word Length = 8 Bits - Stop Bit = 1 Stop Bit - Parity = No Parity - Hardware flow control disabled (RTS and CTS signals) - Receive and transmit enabled */ USART_DeInit(USART1); USART_InitStructure.USART_BaudRate = 115200; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_Init(USART1, &USART_InitStructure);/* Enable the USART1 */
USART_Cmd(USART1, ENABLE); while(1) { while(USART_GetFlagStatus(USART1, USART_FLAG_RXNE) == RESET ); receive_data = USART_ReceiveData(USART1) & 0xFF; USART_SendData(USART1, receive_data); while(USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET ); if( receive_data == 'x' ) break; } }So I concluded that I had a problem with interrupt, but I couldn't find the reason. Please help me. Thank you
#interrupt #stm32f3732016-10-26 10:16 PM
Why are you enabling the usart twice? that doesn't seem right.
''If I send any character to STM, then it would receive it and send back to my computer. But I couldn't receive anything.'' Can you clarify? So with the interrupt code its not receiving anything. If you put a breakpoint on top if of IRQhandler it never goes there?2016-10-26 11:06 PM
Dear jpr.thm,
I removed one USART enabling code, but it still did't work.
''If I send any character to STM, then it would receive it and send back to my computer. But I couldn't receive anything.''
-> STM is connected with my computer by USB driver, and when I send any character by PC to STM through USART communication, then STM received it, and sent it back to my computer. So if this code works correctly, I can receive a character which I just sent to STM by universalcomm. I could verify it by USART polling method code, but when I used USART interrupt method code, it failed.
Yes, if I put a breakpoint on top if of IRQhandler it never goes there.
2016-10-27 5:04 AM
Hiyang.seungman,
Try to enable the TX/RX transfer interrupt just after enabling the USART and manage then the Tx and RX transfer sequensetly using interrupt flags . The ''USART_HyperTerminalInterrupt'' example in STM32F3xxstandard library is a helpful example for you. I will give you a brief helpful description that help you to implement correctly you USART transfer code. Like the following: in main.c file: you main function would be like following model:...
USART_init();
/* Enable USART */
USART_Cmd(USART1, ENABLE);
/* Enable the USART1 Transmoit interrupt: this interrupt is generated when the
EVAL_COM1 transmit data register is empty */
USART_ITConfig(USART1, USART_IT_TXE, ENABLE);
/* Wait until USART1 send the TxBuffer */
while(TxCounter < NbrOfDataToTransfer)
{}
/* The software must wait until TC=1. The TC flag remains cleared during all data
transfers and it is set by hardware at the last frame’s end of transmission*/
while (USART_GetFlagStatus(USART1, USART_FLAG_TC) == RESET)
{}
/* Enable the USART1 Receive interrupt: this interrupt is generated when the
EVAL_COM1 receive data register is not empty */
USART_ITConfig(USART1, USART_IT_RXNE, ENABLE);
/* Wait until USART1 receive the RxBuffer */
while(RxCounter < NbrOfDataToRead)
{}
with the golobal variable:
extern __IO uint32_t TxCounter;
extern __IO uint32_t RxCounter;
Then , in STM32F3xx_it.c file you , your USART1_IRQHandler() will be like following:
void USART1_IRQHandler(void)
{
if(USART_GetITStatus(USART1, USART_IT_RXNE) != RESET)
{
/* Read one byte from the receive data register */
RxBuffer[RxCounter++] = (USART_ReceiveData(USART1) & 0x7F);
if(RxCounter == NbrOfDataToRead)
{
/* Disable the USART1 Receive interrupt */
USART_ITConfig(USART1, USART_IT_RXNE, DISABLE);
}
}
if(USART_GetITStatus(USART1, USART_IT_TXE) != RESET)
{
/* Write one byte to the transmit data register */
USART_SendData(USART1, TxBuffer[TxCounter++]);
if(TxCounter == NbrOfDataToTransfer)
{
/* Disable the USART1Transmit interrupt */
USART_ITConfig(USART1, USART_IT_TXE, DISABLE);
}
}
}
with defining the following variable in the STM32F3xx_it.c file :
#define TXBUFFERSIZE (countof(TxBuffer) - 1)
#define RXBUFFERSIZE 0x20
/* Private macro -------------------------------------------------------------*/
#define countof(a) (sizeof(a) / sizeof(*(a)))
/* Private variables ---------------------------------------------------------*/
uint8_t TxBuffer[] = ''
USART Hyperterminal Interrupts Example: USART-Hyperterminal\
communication using Interrupt
'';
uint8_t RxBuffer[RXBUFFERSIZE];
uint32_t NbrOfDataToTransfer = TXBUFFERSIZE;
uint32_t NbrOfDataToRead = RXBUFFERSIZE;
__IO uint32_t TxCounter = 0;
__IO uint32_t RxCounter = 0;
Hope it is clear for you.
-Hannibal-