cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F303RE Nucleo Board HAL_USART_Receive_IT problem

AWeis
Associate

As the title suggests, im having a problem using HAL to make some USART echo.

I tried the same approch on a nucleo-f031 and its working wonderfully.

I can print the whole hyperterminal string, but i cant reach the receive interrupt. Even if i set the RXNEIE bit manually it doesnt trigger the USART2 interrupt.

Just to clarify, i bridged both connection SB62 and SB63 so i can see the USART communication on a logic analyzer.

im hoping for help

0 REPLIES 0