cancel
Showing results for 
Search instead for 
Did you mean: 

The option bytes are not being written in STM32L433

Seiji_Hiraki
Associate II

I would like to enable write protection via an option byte.

However, HAL_FLASH_OB_Launch() hangs, and even if the CPU is reset afterwards, the option byte is not rewritten.

This issue occurs with both combinations: my board + J-Link or Nucleo + ST-Link.

I have the following function to set the option bytes:

 

void set_write_protection(uint32_t WRPArea, uint32_t start, uint32_t end)
{
    FLASH_OBProgramInitTypeDef OBInit;
    HAL_StatusTypeDef status;

	HAL_FLASH_Unlock();
	HAL_FLASH_OB_Unlock();
	OBInit.WRPArea = WRPArea;
    HAL_FLASHEx_OBGetConfig(&OBInit);
    if (OBInit.WRPStartOffset != start || OBInit.WRPEndOffset != end) {
    	OBInit.WRPStartOffset = start;
    	OBInit.WRPEndOffset = end;
        OBInit.OptionType = OPTIONBYTE_WRP;
        status = HAL_FLASHEx_OBProgram(&OBInit);
        if (status != HAL_OK) {
            return;
        }
    	HAL_FLASH_OB_Launch();
    }
	HAL_FLASH_OB_Lock();
	HAL_FLASH_Lock();
}

void set_area1_write_protection(uint8_t enable)
{
	if (enable)
		set_write_protection(OB_WRPAREA_BANK1_AREAA, 0x00, 0x20);
 	else
		set_write_protection(OB_WRPAREA_BANK1_AREAA, 0xFF, 0x00);
}

 

Is there any way to successfully enable Write Protection?

 

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Super User

Does it work without the debugger connected? Run the code then connect afterwards and check with STM32CubeProgrammer on the option bytes.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

3 REPLIES 3
TDK
Super User

Does it work without the debugger connected? Run the code then connect afterwards and check with STM32CubeProgrammer on the option bytes.

If you feel a post has answered your question, please click "Accept as Solution".

I checked, but it didn't work without the debugger attached. The problem is still not solved. I'll try some more.

waclawek.jan
Super User

Which STM32?

> HAL_FLASH_OB_Launch() hangs

Where?

JW