2015-07-27 7:51 AM
Hi All,
Why the ADC is work only with the following configuration :
RCC_ADCCLKConfig(RCC_ADC12PLLCLK_Div4);
ADC_CommonInitStructure.ADC_Clock = ADC_Clock_SynClkModeDiv4;
I try to configure as the following:
RCC_HCLKConfig (RCC_SYSCLK_Div1);
ADC_CommonInitStructure.ADC_Clock =ADC_Clock_SynClkModeDiv4
and the ADC stop workingthanks
2015-07-27 8:10 AM
I don't know. Define ''stop working'', the values are wrong, the ADC stops generating EOC's?
May be you can provide a complete/concise example of what you're doing and the speeds of the clocks involved.2015-07-27 3:17 PM
My observations:
There are two clock sources for an ADC, each has its own prescaler. I am not very well versed on the 303, but I think the second prescalar definition needs be as follows:ADC_CommonInitStructure.ADC_Clock =ADC_Clock_
As
ynClkModeDiv4;
Cheers, Hal
2015-07-27 3:31 PM
I think the OP explicitly wants the AHB (Synchronous) clock, and can't understand why the second configuration doesn't work as expected, where as the first one shouldn't, but does.
I'd like to know what the AHB setting is in the first case, but the context is far too narrow to tell what's going on, and I'm not wasting a bunch of my time fabricating a complete example to see if it works for me or not.2015-07-27 11:37 PM
this is the configuration:
void ADC_Configuration(void){ ADC_InitTypeDef ADC_InitStructure; ADC_CommonInitTypeDef ADC_CommonInitStructure; /* HCLK = SYSCLK */ RCC_HCLKConfig(RCC_SYSCLK_Div1); RCC_ADCCLKConfig (RCC_ADC12PLLCLK_Div4); // Enable ADC1 Clock RCC_AHBPeriphClockCmd(RCC_AHBPeriph_ADC12, ENABLE); ADC_StructInit(&ADC_InitStructure); /* Calibration procedure ADC_VoltageRegulatorCmd(ADC1, ENABLE); Delay(0x0FFF); ADC_SelectCalibrationMode(ADC1, ADC_CalibrationMode_Single); ADC_StartCalibration(ADC1);// ADC Calibration... while(ADC_GetCalibrationStatus(ADC1) != RESET ); calibration_valueADC1 = ADC_GetCalibrationValue(ADC1); /* ADC1 configuration ------------------------------------------------------*/ // ADC_CommonStructInit(&ADC_CommonInitStructure); ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent; ADC_CommonInitStructure.ADC_Clock = ADC_Clock_SynClkModeDiv4; ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled; ADC_CommonInitStructure.ADC_DMAMode = ADC_DMAMode_OneShot; ADC_CommonInitStructure.ADC_TwoSamplingDelay = 0; ADC_CommonInit(ADC1, &ADC_CommonInitStructure); ///////////////////////////////////////////////////// // ADC_InitStructure.ADC_ContinuousConvMode = ADC_ContinuousConvMode_Disable; ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b; ADC_InitStructure.ADC_ExternalTrigConvEvent = ADC_ExternalTrigConvEvent_3; // TIMER2 exetrnal trigger.... ADC_InitStructure.ADC_ExternalTrigEventEdge = ADC_ExternalTrigEventEdge_RisingEdge; ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Left; ADC_InitStructure.ADC_OverrunMode = ADC_OverrunMode_Disable; ADC_InitStructure.ADC_AutoInjMode = ADC_AutoInjec_Disable; ADC_InitStructure.ADC_NbrOfRegChannel = 4; ADC_Init(ADC1, &ADC_InitStructure); /* ADC1 regular channel1 configuration */ // The Sensor analog in channels are wired counter logic. // The following lines puts them in their ''correct'' respective places. ADC_RegularChannelConfig(ADC1, ADC_Channel_1,2, ADC_SampleTime_7Cycles5); ADC_RegularChannelConfig(ADC1, ADC_Channel_2,1, ADC_SampleTime_7Cycles5); ADC_RegularChannelConfig(ADC1, ADC_Channel_3,4, ADC_SampleTime_7Cycles5); ADC_RegularChannelConfig(ADC1, ADC_Channel_4,3, ADC_SampleTime_7Cycles5); }void DMA_Config(void){ DMA_InitTypeDef DMA_InitStructure; /* Enable DMA1 clock */ RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1, ENABLE); DMA_StructInit(&DMA_InitStructure); /* DMA1 channel1 configuration ----------------------------------------------*/ DMA_DeInit(DMA1_Channel1);//!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!! DMA_InitStructure.DMA_PeripheralBaseAddr = (u32)ADC1_DR_Address; DMA_InitStructure.DMA_MemoryBaseAddr = (u32)ADC_DualConvertedValueTab; DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralSRC; DMA_InitStructure.DMA_BufferSize = (512>> 1 ); DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable; DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord; DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord; DMA_InitStructure.DMA_Mode = DMA_Mode_Circular; DMA_InitStructure.DMA_Priority = DMA_Priority_VeryHigh; DMA_InitStructure.DMA_M2M = DMA_M2M_Disable; DMA_Init(DMA1_Channel1, &DMA_InitStructure);//// DMA_Cmd(DMA1_Channel1, ENABLE);//enable DMA }void DMA1_Channel1_IRQHandler(void){ u8 *adcPtr; if (DMA_GetITStatus(DMA1_IT_HT1)) { numBytesRead = DMA_GetCurrDataCounter(DMA1_Channel1); adcPtr=(u8 *)((u32)ADC_DualConvertedValueTab ); DMA_ClearFlag(DMA1_FLAG_HT1); DMA_ClearITPendingBit(DMA1_IT_HT1); } if (DMA_GetITStatus(DMA1_IT_TC1)) { numBytesRead = DMA_GetCurrDataCounter(DMA1_Channel1); adcPtr=(u8 *)((u32)ADC_DualConvertedValueTab + (ADC_VAL_SIZE/2)); DMA_ClearFlag(DMA1_FLAG_TC1); DMA_ClearITPendingBit(DMA1_IT_TC1); } When the RCC_ADCCLKConfig (RCC_ADC12PLLCLK_Div4); removed then the ADC stop generating EOC's.thanks2015-07-28 4:19 AM
Hiioeoa.001,
If you want to use AHB as clock source for ADC input clock, you have to use:RCC_ADCCLKConfig(RCC_ADC12PLLCLK_OFF);
and not remove the call for
RCC_ADCCLKConfig (RCC_ADC12PLLCLK_Div4);
-Mayla-
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2015-07-28 5:45 AM
Hi Mayla,
I add theRCC_ADCCLKConfig(RCC_ADC12PLLCLK_OFF); after the
RCC_ADCCLKConfig (RCC_ADC12PLLCLK_Div4);
The ADC stop generating EOC's.2015-07-28 8:27 AM
Sorry, it seems that my answer created some confusion.
In fact, if you need the synchronous mode (The ADC clock derived from the AHB clock), you callRCC_ADCCLKConfig(RCC_ADC12PLLCLK_OFF); And you select value for ADC_Clock parameter:ADC_Clock_SynClkModeDiv1 orADC_Clock_SynClkModeDiv2 orADC_Clock_SynClkModeDiv4.
If you need to use PLL as clock source (ADC in asynchronous mode),you call
RCC_ADCCLKConfig(RCC_ADC12PLLCLK_Div4); //Div1 to Div256 And you select value for ADC_Clock parameter:ADC_Clock_AsynClkMode
-Mayla-
RCC_ADCCLKConfig(RCC_ADC12PLLCLK_OFF);
and
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2015-07-29 11:31 PM