cancel
Showing results for 
Search instead for 
Did you mean: 

Hal driver error 258

dooz
Associate II
Posted on July 17, 2015 at 12:48

Hello,

A few days ago I started my adventure with stm32 microcontrollers. To be able to programm them easly I downloaded CubeMX  from this side

http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1533/PF259242?sc=stm32cube#

and of course something for debugging which is system workbench for stm32

http://www.openstm32.org/System+Workbench+for+STM32

Everything was going smoothly. I created my first project in CubeMX, chose IDE SW4STM32 in >>project >>settings (it downloaded some libraries) and saved in a workspace. Then I opened a Workbench for stm32, imported that project and clicked a debugging hammer. Unfortunatelly I got one error but I totally don't know what it is about.  

make all

Building file: C:/Users/Dominik/Documents/Test1/Drivers/STM32F3xx_HAL_Driver/Src/stm32f3xx_hal.c

Invoking: MCU GCC Compiler

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -D__weak=__attribute__((weak)) -D__packed=__attribute__((__packed__)) -DUSE_HAL_DRIVER -DSTM32F303xC -I..\..\..\Inc -I..\..\..\Drivers\STM32F3xx_HAL_Driver\Inc -I..\..\..\Drivers\CMSIS\Include -I..\..\..\Drivers\CMSIS\Device\ST\STM32F3xx\Include -Os -g3 -Wall -fmessage-length=0 -ffunction-sections -c -MMD -MP -MF''Drivers/STM32F3xx_HAL_Driver/stm32f3xx_hal.d'' -MT''Drivers/STM32F3xx_HAL_Driver/stm32f3xx_hal.d'' -o ''Drivers/STM32F3xx_HAL_Driver/stm32f3xx_hal.o'' ''C:/Users/Dominik/Documents/Test1/Drivers/STM32F3xx_HAL_Driver/Src/stm32f3xx_hal.c''

/usr/bin/sh: -c: line 1: syntax error near unexpected token `-D__weak=__attribute__(('

/usr/bin/sh: -c: line 1: `arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -D__weak=__attribute__((weak)) -D__packed=__attribute__((__packed__)) -DUSE_HAL_DRIVER -DSTM32F303xC -I..\..\..\Inc -I..\..\..\Drivers\STM32F3xx_HAL_Driver\Inc -I..\..\..\Drivers\CMSIS\Include -I..\..\..\Drivers\CMSIS\Device\ST\STM32F3xx\Include -Os -g3 -Wall -fmessage-length=0 -ffunction-sections -c -MMD -MP -MF''Drivers/STM32F3xx_HAL_Driver/stm32f3xx_hal.d'' -MT''Drivers/STM32F3xx_HAL_Driver/stm32f3xx_hal.d'' -o ''Drivers/STM32F3xx_HAL_Driver/stm32f3xx_hal.o'' ''C:/Users/Dominik/Documents/Test1/Drivers/STM32F3xx_HAL_Driver/Src/stm32f3xx_hal.c'''

make: *** [Drivers/STM32F3xx_HAL_Driver/stm32f3xx_hal.o] Error 258

During my Internet research I found this article: 

http://www.openstm32.org/forumthread701

I did the same thing as described above but it didn't help.

Please help me with this matter. What am I doing wrong?

I guess the problem lays in connection between CubeMX and eclipse and it is about linking libraries. But I have no idea how to fix it.

Im using a 64 bit Windows 7, I also have Java 64bit installed.

Please help

Regards

Dominik O.

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
stm32cube-t
ST Employee
Posted on July 24, 2015 at 10:51

Dear user,

Unfortunately we are facing several issues that will be fixed asap in our next release.

Please edit your .cproject file and make the following changes:

Replace (~line 28):

<builder buildPath=''${workspace_loc:/$(PROJECT_NAME)}/Debug'' id=''cdt.managedbuild.builder.gnu.cross.997189082'' superClass=''cdt.managedbuild.builder.gnu.cross'' />

with :

<builder buildPath=''${workspace_loc:/cubemx_f0}/Debug'' id=''fr.ac6.managedbuild.builder.gnu.cross.997189082'' keepEnvironmentInBuildfile=''false'' managedBuildOn=''true'' name=''Gnu Make Builder'' superClass=''fr.ac6.managedbuild.builder.gnu.cross''>

<outputEntries>

<entry flags=''VALUE_WORKSPACE_PATH|RESOLVED'' kind=''outputPath'' name=''Debug''/>

<entry flags=''VALUE_WORKSPACE_PATH|RESOLVED'' kind=''outputPath'' name=''Release''/>

</outputEntries>

</builder>

Replace (~ligne 87) :

<storageModule moduleId=''refreshScope'' versionNumber=''2''>

<configuration artifactName=''cubemx_proj Configuration'' configurationName=''Debug''>

<resource resourceType=''PROJECT'' workspacePath=''/STM32072B_EVAL'' />

</configuration>

<!--configuration configurationName=''Release''>

<resource resourceType=''PROJECT'' workspacePath=''/STM32072B_EVAL''/>

</configuration-->

</storageModule>

with :

<storageModule moduleId=''refreshScope'' versionNumber=''2''>

<configuration artifactName=''cubemx_proj Configuration'' configurationName=''Debug''>

<resource resourceType=''PROJECT'' workspacePath=''/$(NOM_PROJET)'' />

</configuration>

<!--configuration configurationName=''Release''>

<resource resourceType=''PROJECT'' workspacePath=''/$(NOM_PROJET)''/>

</configuration-->

</storageModule>

Edit also the .project file:

In the .project file, in the linkedRessources description there is an empty link , remove it as it causes parsing error when import the project:

<link>

<name />

<type />

<location />

</link>

Best regards.

dooz
Associate II
Posted on July 24, 2015 at 15:15

Thank you for your reply. I did not changed the lines as you described above because I was in a great need of working environment for stm32 so I just reinstalled my system and surprisingly it helped. It's working fine now.

Thank you again

Dominik O.

bernieserver
Associate II
Posted on July 30, 2015 at 10:52

Hello,

I have the exactly same problem as described above.

Editing the project files did not help.

Previously it was working fine for weeks (CubeMX F1x 1.0 with STM32F103 chip and SW4STM32). I think something went wrong after migrating to newer version of System Workbench (1.3.0.20150724 ) and to newest CubeMX 4.9.0 and its F1 lib 1.1.