2015-03-17 02:35 AM
Hi,
i try to do some eeprom emulation and got crashes with the stm32f3 eeprom emulation code. now i do it by hand an found that it crahses on the page erase..in detail its when it starts the erase so on FLASH->CR |= FLASH_CR_STRT;its running at 72Mhz.. the crasy thing is that it workes one time if the page is already empty.. so when i do a full flash erase while programming it it workes 1 time but if there is something written on the page it crashes..i tried:- enabling the HSI- differend flash latencys- interrupt disablewithout a result..maybe im missing something .. any help would be nice 🙂2015-03-17 05:46 AM
i fixed it with disabling uart2 for the moment i erase the page. dont ask me why..
regardsFelix2015-03-17 07:35 AM
You're the second person I recall complaining about such an issue.
No much mileage here on the F3's, but generally the processor stalls when executing/erasing flash, it will crash if you erase the code that's being executed, or the vector table. Check you're not hard faulting, or otherwise breaking the system with a debugger.