2015-07-12 5:48 PM
I'm trying to configure my sys clock to be 72MHz but I'm not clear on how to do this. In the system file has this:
/* PLL configuration: PLLCLK = HSI/2 *16 = 64 MHz Max frequency on PLL HSI mode*/ RCC->CFGR &= (uint32_t)((uint32_t)~(RCC_CFGR_PLLSRC | RCC_CFGR_PLLMULL)); RCC->CFGR |= (uint32_t)(RCC_CFGR_PLLSRC_HSI_Div2 | RCC_CFGR_PLLMULL16);But in this migration document it says the F30xx should be capable of 72MHz. In STM32F30xxD/E, we can reach the maximum system clock 72 MHz when PLL is systemclock source and PLL clock source is the HSI. In STM32F1 and other STM32F3 seriesdevices, when PLL clock source is the HSI, the maximum system clock value is 64 MHz.''Which of these two is correct?2015-07-12 7:00 PM
At the end of the day it's going to be limited by the maximum multiplier of the PLL, usually X16, if you're starting from 4 MHz (HSI/2) then the inherent maximum is going to be 64 MHz.
With an HSE of 8 MHz and a multiplier of X9 you can get to 72 MHzWhy does the HSI have to be divided by 2? Probably because it has a highly asymmetrical duty cycle. If you divide by 2 you get 50/50 duty.2015-07-12 7:16 PM
Say x16 PLL here
http://www.st.com/web/en/catalog/mmc/FM141/SC1169/SS1576/LN1824/PF259027
http://www.st.com/st-web-ui/static/active/en/resource/technical/document/datasheet/DM00093333.pdf
Say x16 herehttp://www.st.com/web/en/catalog/mmc/FM141/SC1169/SS1576/LN1824/PF253741
STM32F302ZDhttp://www.st.com/web/en/catalog/mmc/FM141/SC1169/SS1576/LN1824/PF261211
http://www.st.com/st-web-ui/static/active/en/resource/technical/document/datasheet/DM00133117.pdf
Reference ManualPg 191 suggests a source of HSI and HSI/2 are supported in D/E parts''Bits 16:15 PLLSRC: PLL entry clock source (STM32F302xD/E only)''2015-07-12 7:21 PM
2015-07-14 6:26 AM
Hi bujak.dan,
To confirm and conclude about the Max SysClock when PLL clock source is HSI: If you are using the STM32F3xxxD/E, the maximum is 72 MHz.However, for other STM32F3 parts, the maximum sysclock that you may reach with HSI as PLL clock source is 64 MHz.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.