2018-01-12 12:39 AM
Hey,
in my current ADC code I use the PLL as clock source (72MHz). That causes a problem in the powersave mode, where the PLL is disabled and the clock source of the mcu core is just HSE (12 MHz).
Now I want to use the AHB clock instead of the PLL clock but it's simply not working.
Here an overview of my current pll adc code:
[code]
//GPIO Init
RCC->AHBENR |= RCC_AHBENR_GPIOAEN ; GPIOA->MODER |= GPIO_MODER_MODER0;//CLK Init
RCC->CFGR2 |= RCC_CFGR2_ADCPRE12_DIV8; //PLL Clk / 4 RCC->AHBENR |= RCC_AHBENR_ADC12EN;//Calibration
ADC1->CR &= ~ADC_CR_ADVREGEN; ADC1->CR |= ADC_CR_ADVREGEN_0; ADC1->CR &= ~ADC_CR_ADCALDIF; ADC1->CR |= ADC_CR_ADCAL; while (ADC1->CR & ADC_CR_ADCAL);set_saved_vref_cal_value( *((volatile t_u16*)(0x1FFFF7BA)));
//Enable ADC
do { ADC1->CR |= ADC_CR_ADEN; } while ((ADC1->ISR & ADC_ISR_ADRD) == 0);//Config ADC
ADC1->CFGR &= ~ADC_CFGR_RES; //12bit resolution ADC1->CFGR |= ADC_CFGR_CONT; //ADC_ContinuousConvMode_Enable ADC1->CFGR &= ~ADC_CFGR_ALIGN; // Right data alignment ADC1->SQR1 |= ADC_SQR1_SQ1_0; //ADC Channel In1 (PA0) ADC1->SQR1 |= ADC_SQR1_SQ2_4; //ADC Channel 16 Temperature Sensor ADC1->SQR1 |= ADC_SQR1_SQ3_4 | ADC_SQR1_SQ3_1; //ADC Channel 18 VRef Voltage ADC1->SQR1 &= ~ADC_SQR1_L; // reset active channels ADC1->SQR1 |= ADC_SQR1_L_1 | ADC_SQR1_L_0; //Set active channel count to 3ADC1_2->CCR = ADC12_CCR_VREFEN | ADC12_CCR_TSEN;
ADC1->SMPR1 |= ADC_SMPR1_SMP0_2 | ADC_SMPR1_SMP0_1 | ADC_SMPR1_SMP0_0; //Sampling
ADC1->SMPR2 |= ADC_SMPR2_SMP16_2 | ADC_SMPR2_SMP16_1 | ADC_SMPR2_SMP16_0; ADC1->SMPR2 |= ADC_SMPR2_SMP18_2 | ADC_SMPR2_SMP18_1 | ADC_SMPR2_SMP18_0;ADC1->IER = ADC_IER_EOC;
NVIC_SetPriority(ADC1_IRQn, 0);
NVIC_EnableIRQ(ADC1_IRQn);[/code]
I tried a lot with the clk init part without success. As I saw in the manuel the RCC->CFGR2 must be set to zero (bits 8:4) to use the AHB clock. I also change the ADC1_2->CCR Register and use CKMode - but it's not working, the adc always stuck at the init part.
Could someone please show me how to use the AHB clock?
#adc-clock #enable-adc #pll #ahb #stm32-f32018-01-14 8:34 PM
Hi, not very sure what do you mean.
ADC clock is only
asynchronous
orsynchronous
with the AHB clk.AHB clock itself is not for sampling and conversion.
Note that in your Enable ADC part of code,
you check the
ADC_ISR_ADRD flag.
If you want to do this, make sure your set the interrupt flag
ADRDYIE too.
Otherwise you just wait for few usec for ADC to get stablized.
Good Luck!
.Zt
2018-02-02 8:11 AM
Well to make it short and simple:
- In 'normal mode' I use the PLL (72MHz) and everything works fine
- In my 'powersave mode', I disable the PLL to save energy and the MCU uses the HSE source (12 MHz) -> ADC not working anymore
So the question is how to fix/change the code that the ADC is working with source HSE @12MHz?
2018-02-04 12:49 AM
Reset and clock stop the ADC just before you change the ADC clock, and after the clock source being stable and changed, configure the ADC from scratch as it was done the first time after power on reset.
For test: check if you can boot and start the ADC after power on reset in 12MHz mode. If it doesn't debug first this step.
2018-02-05 8:41 AM
Well the ADC is not running. I try to init the ADC directly after mcu reset.
- PLL is diabled, AHB/HCLK is my HSE Clk / 4 (3 MHz)
- I use the define ADC12_CCR_CKMODE_1, because manuel says: 'This configuration must be enabled only if the AHB clock prescaler is set to 1'. So I try to use ADC12_CCR_CKMODE_1 but ofc no success.
RCC->CFGR2 &= RCC_CFGR2_ADCPRE12_NO;
ADC1_2->CCR |= ADC12_CCR_CKMODE_1; RCC->AHBENR |= RCC_AHBENR_ADC12EN;(also tried it with some small delays between the commands to be sure enough time to startup)