2014-10-15 3:41 AM
2014-10-15 5:56 AM
Hi,
Please Format Code Block - Paintbrush [<>] icon, upper left of Word-in-a-box(tm) interface..Regards,Heisenberg.2014-10-15 8:18 AM
No, that would appear to be a Fail!
It does not support HTML, copy and paste the code directly out of your editor/IDEYou know you can edit you own posts?2014-10-15 8:36 AM
/**
* @brief Calibration and initialisation phases for the ADC1 in differential mode * @param None * @retval None */void calibrate_Diff_ADC1 (void){ uint32_t calibration_value=0; ADC1 ->CR &= ~ADC_CR_ADVREGEN_1; //ADC1 voltage regulator enabled ADC1 ->CR |= ADC_CR_ADVREGEN_0; uSec_Delay(10); //ADC1 voltage regulator startup time ADC1 ->CR &= ~ADC_CR_ADCALDIF; //single mode for calibration ADC1 ->CR |= ADC_CR_ADCAL; //start the calibration of the ADC1 while (ADC1 ->CR & ADC_CR_ADCAL){} //wait until calibration done ADC1 ->CR |= ADC_CR_ADCALDIF; //differential mode for calibration ADC1 ->CR |= ADC_CR_ADCAL; //start the calibration of the ADC1 while (ADC1 ->CR & ADC_CR_ADCAL){} //wait until calibration done calibration_value = ADC1 ->CALFACT; ADC1_2 ->CCR &= ~ADC12_CCR_MULTI; //common register: independent mode ADC1_2 ->CCR &= ~ADC12_CCR_CKMODE; //common register: asynchronous clock mode ADC1_2 ->CCR &= ~ADC12_CCR_MDMA; //common register: direct memory access mode disabled ADC1_2 ->CCR &= ~ADC12_CCR_DMACFG; //common register: one shot mode selected ADC1_2 ->CCR &= ~ADC12_CCR_DELAY; //common register: 1*TADC_CLK delay between 2 sampling phases ADC1 ->CFGR |= ADC_CFGR_CONT; //continuous conversion mode ADC1 ->CFGR &= ~ADC_CFGR_RES; //12-bit data resolution ADC1 ->CFGR &= ~ADC_CFGR_EXTEN; //hardware trigger detection disabled ADC1 ->CFGR &= ~ADC_CFGR_ALIGN; //right data alignment ADC1 ->CFGR &= ~ADC_CFGR_OVRMOD; //preserves ADC_DR with the old data when an overrun is detected ADC1 ->CFGR &= ~ADC_CFGR_AUTDLY; //auto-delayed conversion mode off ADC1 ->CFGR &= ~ADC_CFGR_JAUTO; //automatic injected group conversion disabled ADC1 ->CFGR &= ~ADC_CFGR_DISCNUM; //1 regular channels to be converted in discontinuous mode ADC1 ->SMPR1 |= ADC_SMPR1_SMP1_0 //601.5 ADC clock cycles for ADC1_channel1 () | ADC_SMPR1_SMP1_1 | ADC_SMPR1_SMP1_2; ADC1 ->SMPR1 |= ADC_SMPR1_SMP2_0 | ADC_SMPR1_SMP2_1 | ADC_SMPR1_SMP2_2; ADC1 ->SQR1 |= ADC_SQR1_SQ1_0; //1st conversion in regular sequence with channel1 ADC1 ->SQR1 |= ADC_SQR1_L_0; //the total number of conversions: 1 ADC1 ->DIFSEL |= ADC_DIFSEL_DIFSEL_0;//differential mode for channel1 ADC1 ->CR |= ADC_CR_ADEN; //enable ADC1 while (!ADC1 ->ISR & ADC_ISR_ADRD){} //wait for ADC1 to be ready to start conversion ADC1 ->CR |= ADC_CR_ADSTART; //start conversions in continuous mode}/** * @brief Calibration and initialisation phases for the ADC2 in differential mode * @param None * @retval None */void calibrate_Diff_ADC2 (void){ uint32_t calibration_value=0; ADC2 ->CR &= ~ADC_CR_ADVREGEN_1; //ADC2 voltage regulator enabled ADC2 ->CR |= ADC_CR_ADVREGEN_0; uSec_Delay(10); //ADC2 voltage regulator startup time ADC2 ->CR &= ~ADC_CR_ADCALDIF; //single mode for calibration ADC2 ->CR |= ADC_CR_ADCAL; //start the calibration of the ADC2 while (ADC2 ->CR & ADC_CR_ADCAL){} //wait until calibration done ADC2 ->CR |= ADC_CR_ADCALDIF; //differential mode for calibration ADC2 ->CR |= ADC_CR_ADCAL; //start the calibration of the ADC2 while (ADC2 ->CR & ADC_CR_ADCAL){} //wait until calibration done calibration_value = ADC2 ->CALFACT; ADC2 ->CFGR |= ADC_CFGR_CONT; //continuous conversion mode ADC2 ->CFGR &= ~ADC_CFGR_RES; //12-bit data resolution ADC2 ->CFGR &= ~ADC_CFGR_EXTEN; //hardware trigger detection disabled ADC2 ->CFGR &= ~ADC_CFGR_ALIGN; //right data alignment ADC2 ->CFGR &= ~ADC_CFGR_OVRMOD; //preserves ADC_DR with the old data when an overrun is detected ADC2 ->CFGR &= ~ADC_CFGR_AUTDLY; //auto-delayed conversion mode off ADC2 ->CFGR &= ~ADC_CFGR_JAUTO; //automatic injected group conversion disabled ADC2 ->CFGR &= ~ADC_CFGR_DISCNUM; //1 regular channels to be converted in discontinuous mode ADC2 ->SMPR1 |= ADC_SMPR1_SMP7_0 //601.5 ADC clock cycles for ADC1_channel7, clock:36MHz | ADC_SMPR1_SMP7_1 | ADC_SMPR1_SMP7_2; ADC2 ->SMPR1 |= ADC_SMPR1_SMP8_0 | ADC_SMPR1_SMP8_1 | ADC_SMPR1_SMP8_2; ADC2 ->SQR1 |= ADC_SQR1_SQ1_0 //1st conversion in regular sequence with channel7 | ADC_SQR1_SQ1_1 | ADC_SQR1_SQ1_2; ADC2 ->SQR1 &= ~ADC_SQR1_L_0; //the total number of conversions: 1 ADC2 ->DIFSEL|= ADC_DIFSEL_DIFSEL_6; //differential mode for channel7 ADC2 ->CR |= ADC_CR_ADEN; //enable ADC2 while (!ADC2 ->ISR & ADC_ISR_ADRD){} //wait for ADC2 to be ready to start conversion ADC2 ->CR |= ADC_CR_ADSTART; //start conversions in continuous mode}