STM32f2xx could not work with maximum frequency
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-07-03 4:27 AM
I'm using default configuration (according to UM1061, RCC section) to configure an SMT32F215RG to work with 120MHZ CPU clock.
here is my configurations: /* PLL_VCO = (HSE_VALUE or HSI_VALUE / PLL_M) * PLL_N */ #define PLL_M 25 /* For HSE value equal to 25 MHz */ #define PLL_N 240 /* SYSCLK = PLL_VCO / PLL_P */ #define PLL_P 2 /* USB OTG FS, SDIO and RNG Clock = PLL_VCO / PLLQ */ #define PLL_Q 5 /* In this example: PLL_VCO = 240 MHz SYSCLK = 120 MHz */ /***************************************************************/ /* PLL (clocked by HSE) used as System clock(SYSCLK) source */ /***************************************************************/ __IO uint32_t StartUpCounter = 0, HSEStartUpStatus = 0; /* Enable HSE */ RCC_HSEConfig(RCC_HSE_ON); /* Wait till HSE is ready */ HSEStartUpStatus = RCC_WaitForHSEStartUp(); if (HSEStartUpStatus == SUCCESS) { /* Flash 3 wait state, prefetch buffer and cache ON */ FLASH_SetLatency(FLASH_Latency_3); FLASH_PrefetchBufferCmd(ENABLE); FLASH_InstructionCacheCmd(ENABLE); FLASH_DataCacheCmd(ENABLE); /* HCLK = SYSCLK */ RCC_HCLKConfig(RCC_SYSCLK_Div1); /* PCLK2 = HCLK/2 */ RCC_PCLK2Config(RCC_HCLK_Div2); /* PCLK1 = HCLK/4 */ RCC_PCLK1Config(RCC_HCLK_Div4); /* Configure the main PLL clock to 120 MHz */ RCC_PLLConfig(RCC_PLLSource_HSE, PLL_M, PLL_N, PLL_P, PLL_Q); /* Enable the main PLL */ RCC_PLLCmd(ENABLE); /* Wait till the main PLL is ready */ while (RCC_GetFlagStatus(RCC_FLAG_PLLRDY) == RESET) {} /* Select the main PLL as system clock source */ RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK); /* Wait till the main PLL is used as system clock source */ while (RCC_GetSYSCLKSource() != RCC_CFGR_SWS_PLL) {} } else { /* If HSE fails to start-up, user can add here some code to deal with this error */ } for testing that, I'm using a blinking LED (in pooling mode), VDD is 3.3 volts & I use a 25 MHZ quartz. The problem is here that the program does NOT work at all or it begins to work & stops after one or two seconds. I used a debugger to trace it & I found that a Hard Fault occures & execution enters into HardFault_Handler infinity loop of startup_stm32fxx.s I checked the board several times & I'm sure it has no issue, also the same program works fine when I decrease cpu clock to a lower value (by changing PLL params, e.g set PLL_P=4). Seems all frequencies above 100MHZ causes some kind of problem. I guessed it may related to Flash access latency, but according to the datasheet with 3.3V of VDD it must works with 3 wait states & changing wait cycles did not helped me.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-07-03 5:22 AM
That doesn't look like the code provided in the 1.1.0 firmware library.
http://www.st.com/web/en/catalog/tools/PF257898
Use that code, and examples there in for system_stm32f2xx.c SystemInit() and SetSysClock(). If it still fails you need to pay some attention to your board. Check voltages and capacitors on VCAP pinsUp vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-07-03 5:39 AM
Material similar post from the other day [DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/STM32f2xx%20HSI%20configuration%20does%20not%20work%20correctly&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&TopicsView=https%3a//my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/AllItems.aspx¤tviews=33]https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fcortex_mx_stm32%2fSTM32f2xx%20HSI%20configuration%20does%20not%20work%20correctly&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&TopicsView=https%3A%2F%2Fmy.st.com%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2Fcortex_mx_stm32%2FAllItems.aspx¤tviews=33
If the chip isn't working at higher speeds then you're going to want to seriously review the board and the connections. Perhaps you might also want to test on a third-party board, with known/demonstrable function.Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-07-06 6:57 AM
I forgot to put capacitor on VCAP & this causes the issue. Putting a 2.2UF capacitor solved the problem.