STM32F207VGT6 input clock jitter
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-06-11 9:25 AM
Posted on June 11, 2014 at 18:25
Hey,
I'm using theSTM32F207VGT6. I see there is a duty cycle of 45%-55% on the input clock. Is this the same as the jitter spec- can the duty cycle chabge by 10% in a clock cycle and everything will still be OK?
Calum
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0